Arrow Electronics, Inc.

AIX Network Installation Management Concepts and Configuration

CODE: AN22G

LENGTH: 16 Hours (2 days)

PRICE: €1.560,00

Description

The primary goal of this course is to provide you with a working knowledge of the fundamental capabilities of the Network Installation Management (NIM) facility of the AIX 7.1 operating system. This course uses a combination of instructor lecture and machine exercises to provide you with practical background knowledge of the topics covered.

Objectives

  • Explain key NIM concepts and terminology
  • Display NIM-related information
  • Set up a NIM master
  • Perform a base AIX (RTE) install
  • Define and use several types of NIM objects
  • Perform an automated install
  • Create and use mksysb resource
  • Maintain lpp_source and SPOT resources
  • Update NIM clients

Audience

This course is appropriate for anyone with system administrative duties installing and managing an AIX operating system in a multiuser POWER (System p) environment.

Prerequisites

You should have:

  • Basic knowledge regarding AIX systems administration
  • Basic knowledge regarding the use of HMC V7 to manage POWER-based managed systems

The following course will provided the needed skills for this course:

  • Power Systems for AIX I: LPAR Configuration and Planning (AN11G)
  • Power Systems for AIX II: AIX Implementation and Administration (AN12G)

Programme

Day 1

  • Welcome
  • Unit 1: NIM overview
  • Exercise 1: NIM overview
  • Unit 2: Setting up the NIM master
  • Exercise 2: Setting up the NIM master
  • Unit 3: RTE installation
  • Exercise 3: RTE installation
  • Unit 4: Defining additional base install resources

Day 2

  • Exercise 4: Defining additional base install resources
  • Unit 5: NIM client backups and restores
  • Exercise 5: NIM client backups and restores
  • Unit 6: Managing the lpp_source and the SPOT resources
  • Exercise 6: Managing the lpp_source and the SPOT resources
  • Unit 7: NIM client updates
  • Exercise 7: NIM client updates

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price is available to IBMers for GTP delivered courses only. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

05 Jun 2023

Virtual Classroom (GMT / UTC)

BST

English

Instructor Led Online

€ 1.560,00

We also offer sessions in other countries