Arrow Electronics, Inc.

DB2 10 for z/OS Database Administration Part 2

CODE: CV842G

LENGTH: 3 day(s)

PRICE: €2.340,00

Description

This course is a continuation of course DB2 10 for z/OS Database Administration Workshop Part 1 (CV831) and is designed to teach you how to perform additional database administration tasks.

This course replaces DB2 for z/OS Database Administration Workshop Part 2 (CV841). This is the Classroom version of Instructor-led online course DB2 10 for z/OS Database Administration Part 2 - ILO (3V842).

Objectives

  • Execute program preparation steps including resolving common problems, defining collections and packages, and versioning of packages
  • Alter table characteristics such as data types of columns and identify the impact of making such changes
  • Alter indexes to add columns or to change the varying length or clustering characteristics of the index, and identify the impact of making such changes
  • React to the "Advisory Reorg" Database Exception Table state
  • Make appropriate decisions to successfully handle table space versions
  • Given the usage of the data, determine an appropriate option for dealing with the need for adding partitions or rebalancing data partitions
  • Determine the applicability and implement clone tables, user-defined distinct types, user-defined functions, stored procedures, triggers, and large objects

Audience

This intermediate course is for Database Administrators and System Programmers who would like to get insight into database administration tasks. The course lab exercises are performed on a DB2 10 for z/OS environment.

Prerequisites

You should have attended course:

  • DB2 10 for z/OS Database Administration Workshop Part 1 (CV831)

or have attained a similar level of experience.

Programme

Day 1

  • Welcome
  • Unit 1: Transition from DB2 9 for z/OS Database Administration Workshop Part 1 (CV830) to DB2 for z/OS Database Administration Workshop Part 2 (CV841)
  • Unit 2: Program Preparation and Use of Packages
  • Exercise 1: Program Preparation
  • Unit 3: Online Schema Changes
  • Exercise 2: Online Schema Changes

Day 2

  • Unit 4: Clone Tables
  • Exercise 3: Clone Tables
  • Unit 5: Partition Management
  • Exercise 4: Partition Management
  • Unit 6: UDTs and UDFs
  • Exercise 5: UDTs and UDFs

Day 3

  • Unit 7: Stored Procedures
  • Exercise 6: Stored Procedures
  • Unit 8: Triggers
  • Exercise 7: Triggers
  • Unit 9: Large Objects
  • Exercise 8: LOBs

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates