Arrow Electronics, Inc.

VMware Horizon 8: Deploy and Manage plus App Volumes Fast Track

CODE: VMW_HDMAVFT8

LENGTH: 40 Hours (5 days)

PRICE: €5.250,00

Description

This five-day accelerated, hands-on training course is a blend of VMware Horizon® 8: Skills for Virtual Desktop Management, VMware Horizon 8: Infrastructure Administration, and VMware App Volumes™, and VMware Dynamic Environment Manager™. Eight days of content are taught in five-days of extending learning.

This training collection gives you the hands-on skills to deliver virtual desktops and applications through a single virtual desktop infrastructure platform. You build on your skills in configuring and managing VMware Horizon 8 through a combination of lecture and hands-on labs. You learn how to configure and deploy pools of virtual machines and how to provide a customized desktop environment to end-users.

You learn how to install and configure a virtual desktop infrastructure platform. You learn how to install and configure VMware Horizon® Connection Server™ and VMware Unified Access Gateway™. You also learn how to configure a load balancer for use with Horizon and how to establish Cloud Pod Architecture.

Additionally, you learn how to use App Volumes to deliver applications and data to desktops and users in seconds and at scale. You gain skills in managing application life cycles from installation to update and replacement. You also learn how to use Dynamic Environment Manager to provide personalization and dynamic policy configuration across virtual, physical, and cloud-based environments to simplify end-user profile management.

Objectives

By the end of the course, you should be able to meet the following objectives:

  • • Recognize the features and benefits of VMware Horizon
  • • Use VMware vSphere® to create VMs to be used as desktops for VMware Horizon
  • • Create and optimize Windows VMs to create VMware Horizon desktops
  • • Install and configure Horizon Agent on Horizon desktop
  • • Configure and manage the VMware Horizon® Client™ systems and connect the client to a VMware Horizon desktop
  • • Configure, manage, and entitle desktop pools of full VMs
  • • Configure, manage, and entitle pools of instant-clone desktops
  • • Create and use Remote Desktop Services (RDS) desktops and application pools
  • • Monitor the VMware Horizon environment using Horizon Console Dashboard and Horizon Help Desk Tool
  • • Identify Horizon Connection Server installation, architecture, and requirements.
  • • Describe the authentication and certification options for a VMware Horizon environment
  • • Recognize the integration process and benefits of VMware Workspace ONE® Access™ and Horizon 8
  • • Discuss performance and scalability options available in Horizon 8
  • • Describe different security options for the Horizon environment

  • Describe the features and functions of App Volumes and Dynamic Environment Manager
  • • Demonstrate the architectures of App Volumes and Dynamic Environment Manager
  • • Install and configure App Volumes
  • • Create and deploy Application Packages and writable volumes
  • • Install and configure Dynamic Environment Manager
  • • Manage application configurations, user environment settings, and personalization settings

 

Audience

Operators, administrators, and architects for VMware Horizon should enroll in this course. These individuals are responsible for the creation, maintenance, or delivery of remote and virtual desktop services. Additional duties can include the implementation, support, and administration of an organization's end-user computing infrastructure.

Prerequisites

Customers attending this course should have, at a minimum, the following skills:

  • • Use VMware vSphere ® Web Client to view the state of virtual machines, datastores, and networks
  • • Open a virtual machine console on VMware vCenter Server ® and access the guest operating system
  • • Create snapshots of virtual machines
  • • Configure guest customization specifications
  • • Modify virtual machine properties
  • • Convert a virtual machine into a template
  • • Deploy a virtual machine from a template
  • Attendees should also have the following Microsoft Windows system administration experience:

    • • Configure Active Directory services, including DNS, DHCP, and time synchronization
    • • Restrict user activities by implementing Group Policy objects
    • • Configure Windows systems to enable Remote Desktop Connections
    • • Build an ODBC connection to an SQL Server database

    Programme

    1 Course Introduction

    • • Introductions and course logistics
    • • Course objectives

    2 Introduction to VMware Horizon

    • • Recognize the features and benefits of Horizon
    • • Describe the conceptual and logical architecture of VMware Horizon

    3 Introduction to Use Case

    • • Define a use case for your virtual desktop and application infrastructure
    • • Convert customer requirements to use-case attributes

    4 vSphere for Horizon 8

    • • Explain basic virtualization concepts
    • • Use vSphere Client to access your vCenter Server system and VMware ESXi
    ™ hosts
  • • Create, provision, and remove a virtual machine
  • 5 VMware Horizon Desktops

    • • Create a Windows and a Linux virtual machine using vSphere
    • • Optimize and prepare Windows and Linux virtual machines to set up VMware Horizon desktop VMs

    6 VMware Horizon Agents

    • • Outline the configuration choices when installing Horizon Agent on Windows and Linux virtual machines
    • • Create a gold master for Windows Horizon desktops

    7 VMware Horizon Pools

    • • Identify the steps to set up a template for desktop pool deployment
    • • List the steps to add desktops to the Horizon Connection Server inventory
    • • Compare dedicated-assignment and floating-assignment pools
    • • Outline the steps to create an automated pool
    • • Define user entitlement
    • • Explain the hierarchy of global, pool-level, and user-level policies

    8 VMware Horizon Client Options

    • • Describe the different clients and their benefits
    • • Access the VMware Horizon desktop using various VMware Horizon clients and HTML
    • • Configure integrated printing, USB redirection, and the shared folders option
    • • Configure session collaboration and media optimization for Microsoft Teams

    9 Creating and Managing Instant-Clone Desktop Pools

    • • List the advantages of instant clones
    • • Explain the provisioning technology used for instant-clone desktop pools
    • • Set up an automated pool of instant clones
    • • Push updated images to instant-clone desktop pools

    10 Creating RDS Desktop and Application Pools

    • • Explain the difference between an RDS desktop pool and an automated pool
    • • Compare and contrast an RDS session host pool, a farm, and an application pool
    • • Create an RDS desktop pool and an application pool
    • • Access RDS desktops and application from Horizon Client
    • • Use the instant clone technology to automate the build-out of RDSH farms
    • • Configure load-balancing for RDSHs on a farm

    11 Monitoring VMware Horizon

    • • Monitor the status of the VMware Horizon components using the Horizon Administrator console dashboard
    • • Monitor desktop sessions using the HelpDesk tool

    12 Horizon Connection Server

    • • Recognize VMware Horizon reference architecture
    • • Identify the Horizon Connection Server supported features

    • Identify the recommended system requirements for Horizon Connection Server
    • • Configure the Horizon event database
    • • Outline the steps for the initial configuration of Horizon Connection Server
    • • Discuss the ADAM database as a critical component of the Horizon Connection Server installation

    13 VMware Horizon Authentication and Certificates

    • • Compare the authentication options that Horizon Connection Server supports
    • • Describe the Smartcard authentication options that Horizon Connection Server supports
    • • Outline the steps to create a VMware Horizon administrator and custom roles
    • • Describe the roles available in a VMware Horizon environment
    • • Explain the role that certificates play for Horizon Connection Server
    • • Install and configure certificates for Horizon Connection Server
    • • Install and configure True SSO in a VMware Horizon environment

    14 Workspace ONE Access and Virtual Application Management

    • • Recognize the features and benefits of Workspace ONE Access
    • • Recognize the Workspace ONE Access console features
    • • Explain identity management in Workspace ONE Access
    • • Explain access management in Workspace ONE Access
    • • Describe the Workspace ONE Access directory integration
    • • Describe the Workspace ONE Access directory integration
    • • Deploy virtual applications with Workspace services

    15 VMware Horizon Performance and Scalability

    • • Describe the purpose of a replica connection server
    • • Explain how multiple Horizon Connection Server instances in a pod maintain synchronization
    • • Describe the 3D rendering options available in VMware Horizon 8
    • • List the steps to configure graphics cards for use in a VMware Horizon environment
    • • Configure a load balancer for use in a VMware Horizon environment
    • • Explain Horizon Cloud Pod Architecture LDAP replication and VIPA
    • • Explain Horizon Cloud Pod Architecture scalability options

    16 Managing VMware Horizon Security

    • • Explain concepts relevant to secure VMware Horizon connections
    • • Describe how to restrict VMware Horizon connections.
    • • Discuss the benefits of using Unified Access Gateway
    • • List the two-factor authentication options that are supported by Unified Access Gateway
    • • List Unified Access Gateway firewall rules
    • • Describe the situation in which you might deploy Unified Access Gateway instances with one, two, or three network interfaces

    17 Overview of Application and Profile Management

    • • Profile Management
    • • Application Management

    18 Overview of App Volumes

    • • App Volumes components

    19 App Volumes Installation Overview

    • • Requirements
    • • Installing and configuring App Volumes Manager
    • • Installing the App Volumes agent

    20 Working with Application Packages

    • • Packaging Applications
    • • Maintaining Applications

    21 Working with Writable Volumes

    • • Default writable volume templates

    Session Dates

    We also offer sessions in other countries