Arrow Electronics, Inc.

Junos Class of Service

Kód: JUN_JCOS

DÉLKA: 2 (den)

CENA: Kč 45 200,00

Popis

Školení je vedeno virtuálně v anglickém jazyce ve školicím středisku Arrow v Anglii.

Cena školení je 1 495 GBP bez DPH - tato cena bude při fakturaci přepočtena aktuálním kurzem.


This two-day course provides students with advanced class-of-service (CoS) knowledge and configuration examples.

The course begins with an overview of CoS before going into classification, policing, scheduling, and rewriting.

The course then covers class based forwarding and finishes with a case study. Through demonstrations and hands-on labs, students will gain experience in configuring and verifying Junos CoS features.

This course is based on the Junos operating system Release 16.2R1.6.

Junos Class of Service (JCOS) is an advanced level course.

Relevant Juniper Product

• Junos OS
• M Series
• MX Series
• PTX Series
• SRX Series
• T Series
• Service Provider Routing and Switching Track

Cíle

• Understand the history and evolution of CoS.
• Identify the CoS fields in various packet headers.
• List the CoS processing stages on devices running the Junos OS.
• Identify the default CoS settings on devices running the Junos OS.
• Configure and verify behavior aggregate (BA) and multifield (MF) classification.
• Configure and verify two-color and tricolor marking policers.
• Configure and verify schedulers and their components.
• Configure and verify the multiple levels of hierarchical schedulers.
• Configure and verify packet header rewriting.
• Configure and verify class-based forwarding.
• Create a CoS configuration based on a set of design requirements.

 

Určeno pro

This course benefits individuals responsible for configuring and monitoring devices running the Junos OS, especially those in a service provider environment. It also benefits individuals responsible for designing networks containing devices running the Junos OS.

Vstupní znalosti

Students should attend the Introduction to the Junos Operating System (IJOS) course and the Junos Intermediate Routing (JIR) course or have equivalent experience prior to attending this class. General knowledge of CoS concepts is also helpful.

Program

Day 1

Course Introduction

CoS Overview
• CoS History and Evolution
• CoS and DiffServ
• CoS Fields in Packet Headers
• CoS Processing

Packet Classification
• Classification Overview
• Forwarding Classes and Packet Loss Priority
• Fixed Classification
• Multifield Classification
• Behavior Aggregate Classification
 
 LAB 1: Configuring Packet Classification
 
 Policing
• Policing Overview
• Single-Rate Two-Color Policer
• Tricolor Marking Policers
• Hierarchical Policers
• Application—Directly on an Interface
• Application—Within a Firewall Filter
 
 LAB 2: Configuring Policers

Scheduling
• Scheduling Overview
• Transmission Rate
• Queue Priority
• Delay Buffers
• Drop Profiles and Drop Profile Maps
• Scheduling Configuration
 
 LAB 3: Configuring Schedulers

Day 2

Hierarchical Scheduling
• Hierarchical Scheduling Overview
• Scheduler Modes
• Hierarchical Scheduling Levels
• Throughput Example
• Remaining Traffic
• Queue Properties in a Hierarchical Scheduling Context
• Putting It All Together
 
 LAB 4: Configuring Hierarchical Schedulers
 
 Rewrite Rules
• Packet Header Rewrite Overview
• Rewrite Rules and Tables
• Rewrite Combinations
 
 LAB 5: Configuring Rewrite Rules

CoS-Based Forwarding
• CBF Overview
• CBF Configuration
 
 LAB 6: Configuring CBF
 
 Please note that the following Appendix/Case Study are not covered as standard during the training course unless requested by the customer, and agreed with Arrow, upon booking:

Appendix A: CoS Processing on M Series, T Series, and MX Series Devices

• M Series and T Series Architecture
• M Series and T Series CoS Packet Handling
• IQ2 PIC CoS Packet Handling
• MX Series (DPC and MPC/MIC) Architecture and CoS Packet Handling

Case Study

• VoIP Case Study Overview
• VoIP Case Study: Ingress Node
• VoIP Case Study: Transit and Egress Nodes
 
 LAB 7: Case Study

Termíny školení