Arrow Electronics, Inc.

Power Systems for AIX - Virtualization II: Advanced PowerVM and Performance

Kód: ZL1_AN31

DÉLKA: 4,5 (den)

CENA: Kč 67 000,00

Popis

You will learn how to implement advanced IBM PowerVM features, such as Active Memory Sharing, Active Memory Expansion, shared dedicated processors, and multiple shared processor pools.

Additionally, you will learn skills to implement, measure, analyze, and tune PowerVM virtualization features for optimal performance on IBM Power Systems servers. This course focuses on the features that relate to the performance of IBM POWER processor-based systems, AIX, and the special monitoring, configuring, and tuning needs of logical partitions (LPARs). This course does not cover application monitoring and tuning.

You will also learn AIX performance analysis and tuning tools that help an administrator take advantage of shared processors and other virtualization features of the IBM Power Systems servers.

Hands-on lab exercises reinforce each lecture and give the students practical experience.

Cíle

  • Describe the effect of the IBM PowerVM virtualization features on performance and monitoring, such as:
    • Simultaneous multithreading (SMT), shared processors, virtual processors, multiple shared processor pools (MSPP), shared dedicated capacity, Active Memory Sharing (AMS), Active Memory Expansion (AME)
  • Interpret the outputs of AIX performance monitoring and tuning tools used to view the impact of features such as SMT, shared processors, additional shared processor pool activations, and device virtualization
  • Configure and monitor Active Memory Expansion
  • Configure the Suspend and Resume and Active Memory Sharing features
  • Implement the deduplication feature of Active Memory Sharing

Určeno pro

This course is for anyone responsible for the system administrative duties implementing and managing virtualization features on a System p server. The audience for this training includes the following:

  • AIX technical support individuals
  • System administrators
  • Systems engineers
  • System architects

Vstupní znalosti

The LPAR prerequisite skills can be met by attending one of the following classes or you can have equivalent LPAR skills:

  • Power Systems for AIX - Virtualization I: Implementing Virtualization (AN30G)

Program

Day 1

  • Welcome
  • Unit 1: PowerVM features review
  • Exercise 1: Introduction to the lab environment
  • Unit 2: Shared processors and virtual processor tuning Exercise 2: Shared processors and virtual processor tuning

Day 2

  • Unit 3: Multiple shared processor pools and donating dedicated processors
  • Exercise 3: Multiple shared processor pools and donating dedicated processors
  • Unit 4: Active Memory Sharing Exercise 4: Active Memory Sharing

Day 3

  • Exercise 4: Active Memory Sharing (continued)
  • Unit 5: Suspend and Resume Exercise 5: Suspend and Resume Unit 6: Active Memory Expansion Exercise 6: Active Memory Expansion

Day 4

  • Unit 7: Virtual storage performance
  • Exercise 7: Virtual storage performance Unit 8: Virtual network performance

Day 5

  • Exercise 8: Virtual network performance
  • Unit 9: Virtualization monitoring and performance management tools Exercise 9: Using the Virtual I/O Server Performance Analysis Reporting Tool
  • Wrap up/Evaluations

Více informací

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price is available to IBMers for GTP delivered courses only. This is the price you will be invoiced for the class.

Termíny školení
Datum
Místo konání
Časové pásmo
Jazyk
Typ
Garance termínu
CENA

13 čvn 2022

Praha

CEDT

Česky

Classroom

Kč 67 000,00

Další termíny školení Arrow v Evropě, včetně virtuálních.