CODE: SPL_SE9DA
LÄNGE: 24 Hours (3 Tage)
PREIS: €2.250,00
This 18-hour course is designed for administrators who are responsible for getting data into Splunk Indexers. The course provides the fundamental knowledge of Splunk forwarders and methods to get remote data into Splunk indexers. It covers installation, configuration, management, monitoring, and troubleshooting of Splunk forwarders and Splunk Deployment Server components
Description
To be successful, students should have a solid understanding of the following courses:
OR the following courses:
Students should also have understand the following course:
Module 1 - Getting Data Into Splunk
Provide an overview of Splunk
Describe the Splunk distributed model
Describe data input types and metadata settings
Configure initial input testing with Splunk Web
Testing indexes with Input Staging
Module 2 - Configuration Files and Apps
Identify Splunk configuration files and directories
Describe index-time and search-time precedence
Validate and update configuration files
Explore Splunk apps and app installation
Module 3 - Configuring Forwarders
Configure Universal Forwarders
Configure Heavy Forwarders
Module 4 - Customizing Forwarders
Configure intermediate forwarders
Identify additional forwarder options
Module 5 - Managing Forwarders
Describe Splunk Deployment Server (DS)
Manage forwarders using deployment apps
Configure deployment clients and client groups
Monitor forwarder management activities
Module 6 - Monitor Inputs
Create file and directory monitor inputs
Use optional settings for monitor inputs
Deploy a remote monitor input
Module 7 - Network Inputs
Create network (TCP and UDP) inputs
Describe optional settings for network inputs
Module 8 - Scripted Inputs
Create a basic scripted input
Module 9 - Agentless Inputs
Configure Splunk HTTP Event Collector (HEC) agentless input
Describe Splunk App for Stream
Module 10 - Operating System Inputs
Identify Linux-specific inputs
Identify Windows-specific inputs
Module 11 - Fine-tuning Inputs
Understand the default processing that occurs during input phase
Configure input phase options, such as source type fine-tuning and character set encoding
Module 12 - Parsing Phase and Data Preview
Understand the default processing that occurs during parsing
Optimize and configure event line breaking
Explain how timestamps and time zones are extracted or assigned to events
Use Data Preview to validate event creation during parsing phase
Module 13 - Manipulating Input Data
Explore Splunk transformation methods
Create rulesets with Ingest Actions
Mask data with Ingest Actions rules
Mask data with SEDCMD and TRANSFORMS
Module 14 - Routing Input Data
Filter data with Ingest Action rules
Route data with Ingest Action rules
Route data with Transforms
Override sourcetype or host based upon event values
Module 15 - Supporting Knowledge Objects
Define default and custom search time field extractions
Identify the pros and cons of indexed time field extractions
Configure indexed field extractions
Describe default search time extractions
Manage orphaned knowledge objects