Uddannelsestilbud

VMware Horizon 7: Install Configure Manage [V7.0]

Information

Pris kr 25.050  Ekskl. moms
Varighed: 5 Dage
Lunch : Included
Courseware : Included
Ref: VMW_HICM7
Delivery Type

Sessionsdatoer

Se sessioner for andre lande
Dato Sted
  • København - Ballerup
    kr 25.050  Ekskl. moms
  • Virtual Classroom (CET / UTC +1)
    kr 25.050  Ekskl. moms
  • Århus - Viby
    kr 25.050  Ekskl. moms
  • København - Ballerup
    kr 25.050  Ekskl. moms
  • Virtual Classroom (CET / UTC +1)
    kr 25.050  Ekskl. moms
  • Århus - Viby
    kr 25.050  Ekskl. moms
Disse oplysninger findes også beregnet for intra-virksomhedsuddannelsen. Tøv ikke med at kontakte os for at få flere oplysninger

Beskrivelse

This five-day, hands-on course gives you the skills to deliver virtual desktops and applications through a single virtual desktop infrastructure (VDI) platform. This course builds your skills in installing, configuring, and managing VMware Horizon® 7 through a combination of lecture and hands-on labs.



This course teaches you how to configure and deploy pools of virtual machines, how to manage access and security of the machines, and how to provide a customized desktop environment to end users.



HUSK! at du kan betale for dette kursus med PSO credit. 

Pris: 42 PSO


Mål

1 Course Introduction

• Review course goals

• Review course objectives

• Review the course outline

• Find additional resources after this course





2 Introduction to VMware Horizon

• Identify the purpose of a virtual desktop infrastructure

• Recognize the features and benefits of VMware Horizon

• Identify the major function of each VMware Horizon component





3 View Connection Server

• Identify the types of servers associated with VMware Horizon

• Access VMware Horizon

• License VMware Horizon components

• Configure View Connection Server





4 VMware Horizon Pools and Desktops

• Outline the process and choices to set up VDI virtual machines:




  •  Assign virtual CPUs and RAM

  • Create Windows 7, Windows 8.x, or Windows 10 virtual machines

  • Configure VMware ESXi™ host virtual switches

  • Optimize the performance of virtual machines





5 Horizon Client Options

• Describe the requirements for a Horizon Client installation

• Explain USB redirection and options

• Describe the power states for desktops

• Define and compare a thin client with a system running Horizon Client





6 Creating Automated Pools of Full Virtual Machines

• Recognize how an automated pool operates

• Compare dedicated-assignment and floating-assignment pools

• Outline the steps to create an automated pool

• Examine the entitlement of desktops in automated pools





7 Creating and Managing Linked-Clone Desktops

• Describe the VMware linked-clone technology

• Explain why both a parent virtual machine and a snapshot must be used to create linked clones

• Outline the system requirements for View Composer

• Describe the relationship between a persistent disk and the system disk





8 Creating and Managing Instant-Clone Pools

• Identify the advantages of instant clones

• Distinguish View Composer clones from instant clones

• Identify the requirements of instant clones

• Outline the steps necessary to set up an automated pool that uses instant clones

• Configure the additional steps that are required for instant clones





9 Creating RDS Desktop and Application Pools

• Explain the difference between an RDS desktop pool and an automated pool

• Describe how a user can access a single application by using the RDS application pool

• Describe the relationship between an RDS host, a farm, and an application pool

• Create an RDS desktop pool and an application pool

• Explain how the View Composer linked-clone technology can automate the build-out of RDS server farms

• Describe the load-balancing options for RDS hosts





10 Advanced VMware Horizon Features

• Describe the purpose of Horizon Administrator

• Describe the objects that can be configured in the Horizon Configuration pages, such as servers, administrators, and global settings

• Explain how restricted entitlements can be used to control a user’s access to pools

• Compare the authentication and security options that View Connection Server supports





11 Managing VMware Horizon Security

• Compare tunnels and direct connections for client access to desktops

• Compare the benefits of using Horizon Security Server or Access Point in the DMZ

• Identify where the tunnel endpoints are in a security server or Access Point implementation

• Identify the tunnel endpoints when the security gateway is not used

• Explain a direct connection

• List the advantages of direct connections





12 Profile Management Using User Environment Manager

• Identify the use cases and benefits of using User Environment Manager

• Prepare the infrastructure for User Environment Manager

• Outline the steps that are required to install and configure the User Environment Manager components

• Use User Environment Manager nanagement console and application profiler to manage user personalization and application configurations





13 Using App Volumes to Provision and Manage Applications

• Explain how App Volumes works

• Identify the features and benefits of App Volumes

• Identify the interface elements of App Volumes

• Install and configure App Volumes





14 Command-Line Tools and Backup Options

• Describe key View Connection Server features that are available as command-line options with the vdmadmin command

• Explain the purpose of kiosk mode for client systems and how it is configured

• Explain why you might want to limit the domains that View Connection Server makes available to end users

• Identify the log locations for each VMware Horizon component





15 VMware Horizon Performance and Scalability

• Describe the purpose of a replica connection server

• Compare a replica server to a standard connection server

• Explain how multiple VMware Horizon servers maintain synchronization

• List several best practices for multiserver deployment in a pod

• Describe how a load-balancing capability might improve VMware Horizon performance


Offentligt

Technical personnel who work in the IT departments of the end-customer companies and people responsible for the delivery of remote or virtual desktop services


Forkundskaber

Customers attending this course should have at a minimum the following VMware infrastructure skills:



• Use VMware vSphere® Web Client to view the state of virtual machines, datastores, and networks

• Open a virtual machine console on VMware vCenter Server® and access the guest operating system

• Create snapshots of virtual machines

• Configure guest customization specifications

• Modify virtual machine properties

• Convert a virtual machine into a template

• Deploy a virtual machine from a template



Attendees should have at a minimum the following Microsoft Windows system administration experience:

• Configure Active Directory services, including DNS, DHCP, and time synchronization

• Restrict users’ activities by implementing Group Policy objects

• Configure Windows systems to allow Remote Desktop Connections

• Build an ODBC connection to an SQL Server database


Program

By the end of the course, you should be able to meet the following objectives:



• Identify VMware Horizon components

• Install and configure View Connection Server

• Install and configure virtual desktops

• Configure and manage VMware Horizon® Client™ systems

• Configure and manage pools of physical and virtual machines

• Configure and manage automated pools of full virtual machines

• Configure and manage pools of linked-clone desktops

• Configure and manage Remote Desktop Services (RDS) pools of desktops and applications

• Use Horizon Administrator to configure the VMware Horizon environment

• Configure secure access to virtual desktops

• Use VMware User Environment Manager™ to manage user personalization and application configurations

• Describe steps to deploy Profile Management

• Use VMware App Volumes™ to provision and manage applications

• Manage the performance and scalability of a VMware Horizon deployment


© 2018 Segment - Arrow ECS. All rights reserved.