Uddannelsestilbud

Mirage [V5.0] and Horizon with View [v6]: Fast Track

Information

Pris kr 38.100  Ekskl. moms
Varighed: 5 Dage
Lunch : Included
Courseware : Included
Ref: VMW_VMHVFT
Delivery Type Classroom

Sessionsdatoer

Disse oplysninger findes også beregnet for intra-virksomhedsuddannelsen. Tøv ikke med at kontakte os for at få flere oplysninger

Beskrivelse

This extended-hours, hands-on training course provides students with skills that they need to deploy a unified image management system using VMware Mirage™ as well as installing, configuring, and managing the VMware Horizon™ View™ component of VMware Horizon™.



Students learn how to configure security, manage images, perform a Windows migration, set up endpoint protection, and perform various management functions with Mirage. Students will also gain practical experience with View concepts through the completion of hands-on labs that include VMware View® Manager™, VMware View® Composer™, and the View security server.



HUSK! at du kan betale for dette kursus med PSO credit. 

Pris: 63 PSO


Mål

1  Course Introduction




  • Introductions and course logistics

  • Course objectives

     



2  Introduction to Mirage




  • Discuss the key concepts of Mirage

  • Describe how Mirage works with Horizon 6

  • Define the main Mirage use cases

  • Discuss Mirage features and benefits

     



3  Components and Architecture




  • Identify the function of each of the Mirage solution components

  • Define the Mirage layers

  • Diagram the Mirage architecture

     



4  Installing and Configuring Mirage




  • Outline the tasks for installing and configuring Mirage

  • Discuss the process for deploying the Mirage client

  • Identify the high-level tasks for upgrading Mirage

     



5  Mirage Security




  • Recognize the architecture and components of the Mirage Gateway server and how they interact

  • Identify tasks for performing SSL configuration on a Mirage system

  • Explain how to configure Mirage load balancing

     



6  Mirage Management Overview




  • Explain how to use the Mirage dashboard and transaction logs to monitor your Mirage system environment

  • Recognize the process for setting up static and dynamic centralized virtual desktop (CVD) collections

  • Explain the main Image Composer functions

  • Describe how Mirage roles are set up and used

     



7  Mirage Web Manager




  • Identify the main installation and configuration tasks for Mirage Web Manager

  • Discuss how to use Mirage Web Manager logs

  • Recognize how to configure SSL on Mirage Web Manager

     



8  Mirage Single Image Management




  • Diagram the layer management lifecycle

  • Explain how to set up a reference machine

  • Recognize the process for capturing and assigning base layers and application layers

     



9  Windows 7 to Windows 8.1 Migration




  • Identify steps for performing a Windows 7 to Windows 8.1 migration and how to monitor the migration process

  • Discuss the backup capabilities of Mirage 

  • Explain the Mirage endpoint disaster recovery options

     



10  Endpoint Protection with Mirage




  • Discuss the backup capabilities of Mirage and how upload policies are used to define backup parameters

  • Explain the Mirage endpoint disaster recovery options

     



11  Working with the Mirage File Portal




  • Explain the process for configuring the file portal

  • Recognize how to configure end-user CVD mapping

  • Describe how to access files using the file portal

     



12  Introduction to Horizon and View




  • Overview of Horizon 6

  • Introduce View features and components

     



13  View Connection Server




  • Install and configure View Connection Server

  • Configure the View events database and syslog server

     



14  View Desktops




  • Prepare virtual machines as View desktops

  • Compare PCoIP and RDP remote display protocols

  • Explain USB redirection and multimedia redirection

  • Install Horizon View Agent in a template

  • Deploy a manual pool and entitle users to access it

     



15  Horizon Client Options




  • Introduce Horizon Client for Windows and Mac OS X 

  • Describe HTML Access, thin clients, and zero clients

  • Configure Virtual Printing with Horizon Client

     



16  Creating and Managing Automated Pools




  • Configure and provision automated pools of desktops

  • Compare dedicated and floating-assignment pools

  • Compare storage options, including VMware Virtual SAN™

     



17  Creating and Managing Linked-Clone Desktop Pools




  • Overview of View Composer operations

  • Deploy and provision linked-clone desktops

  • Compare storage options, including Virtual SAN and tiered storage

  • Manage linked-clone desktops

  • Manage persistent disks

     



18  Creating and Managing RDS Desktop and Application Pools




  • Set up RDS hosts to create a farm

  • Deploy and provision RDS desktop pools

  • Deploy and provision RDS application pools

  • Manage application pools

     



19  Using View Administrator




  • Configure the View environment

  • Compare authentication options for desktop access

  • Manage users, sessions, and policies

  • Implement role-based delegated administration

  • Monitor the View environment 

     



20  Managing View Security




  • Describe recommended network configurations and authentication options

  • Configure the View security server

     



21  View Persona Management




  • Configure user profiles with View Persona Management

  • Describe View Persona Management and Windows roaming profiles

  • Configure a View Persona Management deployment

  • Describe best practices for a View Persona Management deployment

     



22  Command-Line Tools and Backup Options




  • Introduce the vdmadmin utility

  • Describe client systems in kiosk mode

  • Back up the View databases

  • Restore the View databases

     



23  View Performance and Scalability 




  • Describe multiserver deployments to create a pod

  • Explain performance considerations and load balancing for a single pod 

  • Explain Cloud Pod Architecture for multiple View pod deployments


Offentligt

Experienced system administrators and system integrators responsible for deploying Mirage and Horizon with View


Forkundskaber


  • Ability to use VMware vSphere® Client™ to view the state of virtual machines, datastores, and networks

  • Experience accessing the guest operating system from the VMware vCenter Server™ virtual machine console

  • Ability to navigate Windows 7, Windows 8.1, and Windows Server 2008

  • Experience in Microsoft Windows Active Directory administration


Program


  • Describe the key concepts of Mirage

  • Recognize how Mirage fits into the VMware end-user computing vision

  • Identify the main Mirage use classifications

  • Define the function of each of the Mirage solution components

  • Install, configure, and upgrade Mirage

  • Identify the tasks for SSL configuration on a Mirage system

  • Discuss the management functions available in the Mirage Management Console

  • Deploy Mirage to endpoints

  • Explain the tasks for capturing and assigning base layers and application layers

  • Describe methods for performing disaster recovery with Mirage

  • Outline how to plan and perform a mass hardware migration with Mirage

  • Recognize how the file portal is set up and used 

  • Identify View components

  • Install and configure View Connection Server

  • Install and configure virtual machines that become desktops

  • Configure and manage VMware Horizon® Client™ systems

  • Configure and manage pools of existing physical machines

  • Configure and manage automated pools of full virtual machines

  • Configure and manage pools of linked-clone machines

  • Configure and manage RDS pools of desktops and applications

  • Use View Administrator to configure the View environment

  • Configure secure access to View desktops

  • Describe steps to deploy View Persona Management for user profile management

  • Manage performance and scalability of a View deployment


© 2018 Segment - Arrow ECS. All rights reserved.