Uddannelsestilbud

Automating BIG-IP v14

Information

Pris kr 14.900  Ekskl. moms
Varighed: 1.5 Dage
Ref: F5N_BIG-AUTO
Delivery Type

Sessionsdatoer

Disse oplysninger findes også beregnet for intra-virksomhedsuddannelsen. Tøv ikke med at kontakte os for at få flere oplysninger

Beskrivelse

This course introduces network administrators, operators, and DevOps engineers to the foundational and F5 Networks-specific technologies required to automate BIG-IP in public and private clouds. Participants will gain exposure to multiple technologies for a variety of use cases and will have hands-on experience that leave them better prepared to work with and deploy automation in the cloud.

Formål


  • Understand the role of automation for public and private clouds

  • Describe the components of iControl REST calls and how they interact with BIG-IP

  • Stand up and configure BIG-IP applications using iControl REST

  • Describe the major components of Ansible and how the work together to configure BIG-IP

  • Use flow control elements such as conditionals and looping in Ansible Playbooks

  • Stand up and configure BIG-IP applications using Ansible

  • Understand the role of containers and microservices and how they are used in the cloud to create complex applications

  • Create a basic web service application using Docker containers

  • Use BIG-IP to load balance multiple docker containers

  • Use Application Services 3 to declaratively configure BIG-IP applications

  • Describe the source of truth for each lab exercise

Forudsætninger

Students should be familiar with and able to configure basic BIG-IP elements such as:



  • Virtual Servers

  • Pools, Pool Members and Nodes

  • Pool Monitors

  • Basic Virtual Server Profiles


In addition, the following general technical knowledge should be well understood:



  • Layer 3 and 4 TCP/IP networking concepts, including IP addressing and subnetting

  • Layer 2 Ethernet and ARP networking concepts

  • Layer 7 HTTP networking concepts

  • Linux command line and basic Linux commands

  • HTML


Finally, nice-to-have knowledge includes familiarity with programming and/or scripting languages, such as:



  • JavaScript or NodeJS

  • Python

  • Bash

Program


  • Configuring BIG-IP with iControl REST

  • Configuring BIG-IP programmatically with Ansible

  • Introduction to Docker and Microservices

  • Configuring BIG-IP declaratively with Applications Services 3

© 2020 VALit Aps - Arrow ECS. All rights reserved.