Uddannelsestilbud

Configuring BIG-IQ v14

Information

Pris kr 14.900  Ekskl. moms
Varighed: 2 Dage
Ref: F5N_BIG-CFG
Delivery Type

Sessionsdatoer

Se sessioner for andre lande
    På anmodning. Kontakt os venligst
Disse oplysninger findes også beregnet for intra-virksomhedsuddannelsen. Tøv ikke med at kontakte os for at få flere oplysninger

Beskrivelse

This course uses lectures and hands-on exercises to give participants real-time experience in configuring and using the BIG-IQ® product. Students are introduced to BIG-IQ, its interface, and its various functionality. We first look at administering and operating the BIG-IQ system itself, then detail how it is used to remotely manage BIG-IP devices running BIG-IP Local Traffic Manager (LTM). We then look configuring a BIG-IQ Data Collection Device (DCD) system and see how it is used for the remote storage and examination of BIG-IP log events and statistics.

Formål


  • Perform an initial setup, license, and provision of a BIG-IQ system

  • Administer and monitor the BIG-IQ system

  • Manage BIG-IP LTM devices using BIG-IQ

  • Create, deploy, monitor, and report on BIG-IQ configuration changes

  • Create, deploy, monitor, and report on managed BIG-IP device configuration changes

  • Undertake various troubleshooting of the BIG-IQ functionality

  • Perform an initial setup, license, and provision of a BIG-IQ Data Collection Device (DCD)

  • Configure a BIG-IQ to use a BIG-IQ DCD and examine BIG-IP analytical data

Målgruppe

This course is intended for system and network administrators or operators responsible for the installation, setup, configuration, and administration of the BIG-IQ system or management of BIG-IP devices and F5 products running on those devices.

Forudsætninger

Students must complete one of the following F5 prerequisites before attending this course:



  • Administering BIG-IP instructor-led course

-or-



  • F5 Certified BIG-IP Administrator

 


The following general network technology knowledge and experience are recommended before attending any F5 Global Training Services instructor-led course:



  • OSI model encapsulation

  • Routing and switching

  • Ethernet and ARP

  • TCP/IP concepts

  • IP addressing and subnetting

  • NAT and private IP addressing

  • Default gateway

  • Network firewalls

  • LAN vs. WAN

 

Program


  • The installation and setup of the BIG-IQ system

  • An overview of the BIG-IQ product set and its approach to managing BIG-IP devices.

  • Administering the BIG-IQ system and its facilities

  • Managing BIG-IP LTM devices through their discovery and the subsequent central control and deployment of product objects used on these devices

  • BIG-IQ and managed BIG-IP device troubleshooting steps

  • BIG-IQ and managed BIG-IP device monitoring and reporting facilities

  • The installation and setup of a BIG-IQ Data Collection Device (DCD)

  • Logging and examining BIG-IP LTM events via the BIG-IQ DCD

© 2020 VALit Aps - Arrow ECS. All rights reserved.