Uddannelsestilbud

IBM Cognos Planning Analyst: Build Models (V10.1) - SPVC

Information

Pris kr 9.725  Ekskl. moms
Varighed: 5 Dage
Courseware : Included
Ref: J1101G
Delivery Type Self Paced Training

Sessionsdatoer

På anmodning. Kontakt os venligst

Purchase

    BUY Now
    kr 9.725  Ekskl. moms

    Ekskl. moms

Disse oplysninger findes også beregnet for intra-virksomhedsuddannelsen. Tøv ikke med at kontakte os for at få flere oplysninger

Beskrivelse

This is the self paced training version of ''IBM Cognos Planning Analyst: Build Models (V10.1)'' classroom course. IBM Cognos Planning Analyst: Build Models (V10.1) is a five-day, self paced course that teaches modelers how to design and build models for business planning. You will learn the data modeling process and participate in hands-on demos and workshops that illustrate good model design and best practice techniques while learning how to use the product.



If you are enrolling in a Self Paced Virtual Classroom or Web Based Training course, before you enroll, please review the Self-Paced Virtual Classes and Web-Based Training Classes on our Terms and Conditions page, as well as the system requirements, to ensure that your system meets the minimum requirements for this course.



http://www.ibm.com/training/terms

Formål

Please refer to Course Overview for description information.

Målgruppe

This intermediate course is for Modelers.

Forudsætninger

You should have:




  • Knowledge of your organization's data and structure

  • Knowledge of Microsoft Excel

Program

Introduction to IBM Cognos Planning Analyst




  • Examine the components of the IBM Cognos Planning solution

  • Discuss libraries, D-Lists, D-Cubes, and D-Links

  • Create libraries



Create D-Lists and D-Cubes




  • Manually create D-Lists

  • Import D-List items from external sources

  • Modify D-Lists

  • Build D-Cubes



Load Data




  • Determine what can be used as source data

  • Create file maps to assist in loading data

  • Load data from an external source into a D-Cube

  • Load data from one D-Cube to another



Enhance D-Lists and D-Cubes




  • Prevent calculations on a D-List item

  • Control user input using a formatted D-List

  • Use Built-in Functions (BiFs) to calculate data

  • Use time averages in a D-List

  • Use weighted averages in a D-List

  • Apply conditional formulas to a D-List



Distribute Data




  • Use a D Cube to allocate data

  • Summarize D Cube data with Accumulation D Links

  • Populate a D Cube based on text in the target D Cube using Lookup D Links



Create and Distribute an Income Statement




  • Determine the requirements for building and populating an income statement

  • Discuss various methods of depreciation

  • Calculate depreciation using a Built-in Function

  • Export income statement data



Forecast Data




  • Examine the Forecast Built-in Function

  • Build a revised rolling forecast

  • Use various methods to forecast data



Automate Processes




  • Use D List and D Cube update links to update structure and data

  • Create macros to automate the update process

  • Enhance macros functionality

  • Record a macro to perform repetitive tasks



Object Maintenance and Administration




  • Examine IBM Cognos security

  • Add and maintain libraries

  • Apply security to a library or object

  • Add, remove, and modify objects

  • Create copies of objects and libraries

  • Discuss features that affect performance



Use Complex Calculations




  • Move values through periods using the FeedParam Built-in Function

  • Round values using TRound Built-in Function

  • Examine Tier calculations

  • Calculate balances based on profiles



Examine Advanced Concepts




  • Discuss calculation precedence

  • Restructure D Cubes

  • Transfer data within a D Cube

  • Examine cascading allocations



Design for Reporting




  • Explore the tools available for reporting on Planning Analyst data

  • Design a model for reporting purposes

  • Publish objects for external reporting

  • Make published data available for reporting in IBM Cognos

  • Create a report based on Planning Analyst published data

  • Populate a D-Cube using IBM Cognos as a datasource



Enhance Functionality Using the IBM Cognos Planning Analyst Add-in for Microsoft Excel




  • Examine the IBM Cognos Planning Analyst Add-in for Microsoft Excel

  • Build views

  • Update views

  • Create and use templates for data entry

  • Format and customize Microsoft Excel spreadsheets

  • Update reports

  • Examine batch printing



Illustrate the Model Using IBM Cognos Planning Manager




  • Design reports

  • Create a flowchart

  • Link the flowchart to objects in IBM Cognos Planning Analyst

  • Create tables



End-to-End Workshop (Optional)



Use IBM Cognos Planning Analyst with IBM Cognos Planning Contributor (Optional)



Use IBM Cognos Planning Analyst with IBM Cognos Finance (Optional)

© 2019 VALit Aps - Arrow ECS. All rights reserved.