CÓDIGO: ESS10G
DURACIÓN: 24 Hours (3 días)
Precio: €2.500,00
Organizations are compelled to find effective and cost-efficient data security solutions.
Encryption is one of the technologies that enables organizations to reduce the cost, impact and even likelihood of a breach. Encrypting data can help companies meet the stringent mandates of the GDPR, HIPAA and other mandates.
IBM z15 has been designed for pervasive encryption, enabling organizations to encrypt 100% of an organization’s IBM Z critical business data in-flight and at-rest, with no application changes and no impact to SLAs. Encrypting only the data required to meet compliance mandates should be considered a minimum threshold, not a best practice. IBM z15 makes pervasive encryption the new standard in data protection and the foundation of a larger data security and protection strategy.
z/OS is designed to provide new policy-based encryption options that take full advantage of the improvements in the z15 platform. These new capabilities include:
Data set encryption, which is one aspect of pervasive encryption, provides enhanced data protection for many z/OS data sets gives users the ability to encrypt data without needing to make changes to applications to embed encryption APIs within applications.
New z/OS policy controls which make it possible to use pervasive encryption to protect user data and simplify the task of compliance for many z/OS data sets, zFS file systems, and Coupling Facility structures.
Pervasive encryption for IBM Z® is a consumable approach to enable extensive encryption of data in-flight and at-rest to substantially simplify encryption and reduce costs associated with protecting data.
In this course you will learn how to implement Pervasive Encryption in your z/OS installation. The course explores in detail, the various technologies that are involved in z System and z/OS Cryptographic Services, ICSF, RACF and DFSMS access method Services.
In the hands-on exercises, you begin with the setup of your hardware crypto environment (CCA crypto express and CPACF), then you will load and activate your AES master keys, setup ICSF and its Key datasets (CKDS PKDS TKDS), then define your data encryption keys, activate your data set encryption policy, and encrypt your data sets and zFS filesystems.
These exercises reinforce the concepts and technologies being covered in the lectures.
After completing this course, you should be able to:
Describe the components of Pervasive Encryption on z/OS
Explain the role of encryption for data protection
2
Implement hardware crypto on your z System
Load and activate AES Master Keys
Implement and start ICSF
Understand the differences between secure keys clear keys and protected keys
Describe how are key values used for encryption and decryption
Generate, maintain and manage Keys
Setup access to key labels
Setup policy to supply key label (RACF SMS JCL)
Access data in encrypted data sets
Create encrypted data sets - Supplying key labels
Convert existing data sets to encryption
Verify encryption status
Encrypt Data in Transit
Encrypt Data at Rest
Manage data sets, data keys, and key labels
This class is intended for z/OS system programmers and security specialists in charge of designing, implementing and monitoring Pervasive Encryption on z/OS.
General z/OS knowledge, including basic UNIX System Services skills
Basic knowledge of RACF
Curriculum relationship
o [ES66G]
Describe the components of Pervasive Encryption on z/OS
Explain the role of encryption for data protection
2
Implement hardware crypto on your z System
Load and activate AES Master Keys
Implement and start ICSF
Understand the differences between secure keys clear keys and protected keys
Describe how are key values used for encryption and decryption
Generate, maintain and manage Keys
Setup access to key labels
Setup policy to supply key label (RACF SMS JCL)
Access data in encrypted data sets
Create encrypted data sets - Supplying key labels
Convert existing data sets to encryption
Verify encryption status
Encrypt Data in Transit
Encrypt Data at Rest
Manage data sets, data keys, and key labels
The following unit and exercise durations are estimates, and might not reflect every class experience. If the course is customized or abbreviated, the duration of unchanged units will probably increase.
Day 1
(00:30) Welcome
(01:00) Unit 1: Pervasive Encryption Technical Foundation
(01:00) Unit 2: Pervasive Encryption: Planning
(03:00) Unit 3: Pervasive Encryption: Implementation considerations
(01:30) Unit 4: Dataset Encryption Implementation steps
Day 2
(01:00) Exercise 1: Setup and start ICSF
(01:00) Exercise 2: Load and initialize your AES master key and CKDS
(01:00) Unit 5: ICSF and crypto on z/OS
(01:30) Exercise 3: Define your data keys
(02:30) Exercise 4: Implement dataset encryption policy, encrypt/decrypt data sets
Day 3
(03:00) Exercise 5: Operational tasks for managing data sets, data keys, and key labels
(01:30) Unit 6: Key management: ICSF and the Crypto Ecosystem on Z
(01:00) Unit 7: z14 Hardware Encryption Overview and Performance
(01:00) Exercise 6: Master Key Change using ICSF (optional)
(00:30) Exercise 7: Encrypt zFS filesystems (optional)Curriculum relationship