CÓDIGO: ZL1_AN06
DURACIÓN: 2 días
Precio: €1.100,00
This two day non-workshop course is designed to provide continuing education for system administrators who have extensive experience with previous levels of POWER hardware, PowerVM, and AIX. It covers various enhancements to Power hardware and firmware and to the AIX operating system. It starts with an overview of POWER7 architecture and equipment. It then proceeds with discussions on various software and firmware enhancements (ranging from AIX 7.1 TL0 and PowerVM 2.2.0 through AIX 7.1 TL2 and PowerVM 2.2.2). These enhancements include Virtual Fibre Channel port status, Active Memory Deduplication, Active Memory Expansion, 4 thread SMT, and other enhancements to the areas of AIX security, performance, and workload partitions.
To learn only the very latest enhancements, attendance at IBM Technical conferences or symposiums is recommended.
For a workshop course with hands-on lab exercises, attend Power and AIX Enhancements Workshop (AN080). The workshop course will often lag behind POWER7 and AIX 7 - What's New (AN060) in receiving the latest updates, but has the advantage of hands-on exercises. There can be a significant overlap in discussion content between POWER7 and AIX 7 - What's New (AN060) and Power and AIX Enhancements Workshop (AN080), depending upon where these courses are in their update cycles; read the course descriptions carefully. To learn only the very latest enhancements, attendance at IBM Technical conferences or symposiums is recommended.
This advanced course is for anyone responsible for the system administrative duties, including implementing and managing IBM POWER7 or POWER7+ servers running AIX 7.1.
You must have basic AIX, LPAR, and PowerVM system administration experience. The AIX prerequisite can be met by attending one of the following classes or you can have equivalent AIX skills.
The LPAR and PowerVM prerequisite can be met by attending the following class or you can have equivalent LPAR skills.
Day 1
Day 2
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show: