CÓDIGO: ZL1_AN08
DURACIÓN: 3 días
Precio: €1.850,00
This three day workshop course is designed to provide continuing education for system administrators who have extensive experience with previous levels of POWER hardware, PowerVM, and AIX. It covers various enhancements to Power hardware and firmware and to the AIX operating system. It starts with an overview of POWER7 architecture and equipment. It then proceeds with discussions and hands-on exercises on various software and firmware enhancements (ranging from AIX 7.1 TL0 and PowerVM 2.2.0 through AIX 7.1 TL2 and PowerVM 2.2.2). These enhancements include Virtual Fibre Channel port status, Active Memory Deduplication, Active Memory Expansion, 4 thread SMT, and other enhancements to the areas of AIX security, performance, and workload partitions. This is accomplished by discussing the enhancements in each of these followed by hands-on labs which provide additional exposure to the new environment.
For a lecture-only course that covers the same content attend What's New in POWER7 and AIX7 (AN06G).
To learn only the very latest enhancements, attendance at IBM Technical conferences or symposiums is recommended.
This course is intended for anyone responsible for purchasing, managing, and planning an IBM POWER7 server running PowerVM 2.2 or later and the AIX 7.1 or greater operating system.
The audience for this training include the following:
Students must have system administration experience in AIX, LPAR, and PowerVM. The AIX prerequisite can be met by attending one of the following classes or students can have equivalent AIX skills.
The LPAR and PowerVM prerequisite can be met by attending one of the following classes or students can have equivalent LPAR skills.
Day 1
Day 2
Day 3
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show: