Arrow Electronics, Inc.

IBM Sterling Order Management (V9.5) Configuring Participant Modeling, Process Modeling, and User Security

CODE: 6F91G

LENGTH: 24 Hours (3 days)

PRICE: €2 340,00

Description

This course provides students with an understanding of the configurations required to map participants in a supply chain to the corresponding roles in Sterling Order Management. The course also teaches students the process of setting up the Sterling Selling and Fulfillment Foundation business process workflow. This course is primarily designed for developers and implementers.

This course begins with an overview of Sterling Order Management and the business models it supports. The course then describes how to define participants and create organizations and users.  Through a combination of procedural information and exercises, students will learn about topics such as how to assign attributes to the different roles defined in Sterling Order Management and configure user access policies.

The course also covers Process Modeling features, including how to set up a business process workflow for an organization. Students are then introduced to statuses, conditions, transactions, and other components of a process type pipeline. The course then describes how to create a process type pipeline.

Objectives

After completing this course, students should be able to:

  • Map the participant details to their appropriate roles using Application Platform.

  • Create users and configure user security features using Application Platform.

  • Describe Process Modeling.

  • Create the following components:

    • Statuses, Conditions, and Services

    • Events and Event Handlers

    • Actions and Transactions

  • Create pipelines and pipeline determination rules.

Audience

This course is designed to train developers and implementrs.

Prerequisites

None.

Programme

The following topics will be covered during this course:

  • Course Overview
  • Unit 1: Overview of Applications Manager
    • Exercise 1.1: Navigate to Application Platform
  • Unit 2: Configuring Organizations
    • Lesson 2.1: Defining Participants and Roles
    • Lesson 2.2: Creating Organizations
    • Exercise 2.2.1: Create Child Organizations and Department
    • Lesson 2.3: Assigning Attributes to Roles
  • Unit 3: Creating Users and Configuring Access Policies
    • Lesson 3.1: Prerequisites for User Creation
    • Exercise 3.1.1: Create a User Group and Team
    • Lesson 3.2: Configuring Users and Access Policies
    • Exercise 3.2.1: Create a User
  • Unit 4: Case Study
    • Lesson 4.1: Case Study
  • Unit 5: Overview of Process Modeling
    • Lesson 5.1: Overview of Process Modeling
  • Unit 6: Configuration Basics
    • Lesson 6.1: Statuses and Conditions
    • Exercise 6.1.1: Create a Status and Condition
    • Lesson 6.2: Services, Events, Actions, and Transactions
    • Exercise 6.2.1: Create an Action and Service
    • Exercise 6.2.2: Configure Drop-Ship Fulfillment
    • Lesson 6.3: Pipeline Creation and Determination
    • Exercise 6.3.1: Create an Order, Pipeline, and Pipeline Determination Rule
  • Course Wrap Up

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:

http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates