Arrow Electronics, Inc.

IBM Tivoli Network Manager IP Edition 4.2 Operations and Administration

CODE: TN325G

LENGTH: 40 Hours (5 days)

PRICE: €3 900,00

Description

This course covers the installation, configuration, use, customization, integration of Tivoli Network Manager 4.2 with Network Operations Insight, and network monitoring using the Network Manager pollers. The workshop includes approximately 40% lecture and 60% hands-on exercises. The workshop begins with a basic overview of product components and their associated functions. You configure Tivoli Network Manager and perform a full discovery of simulated networks. To further understand the intricacies of the discovery cycle, you customize discovery by changing the behavior of finders and agents. You also learn to create real-time MIB graphs, control polling behavior, connect isolated networks through manual map editing, and use the reporting functions of IBM Tivoli Network Manager. You also learn to use the Network Health Dashboard and create custom dashboards.

Objectives

After you complete this course, you can perform the following tasks: 

  •  Install IBM Tivoli Network Manager 4.2
  •  Navigate the Network Manager interface
  •  Describe discovery in the context of Tivoli Network Manager
  •  Configure and run a network discovery
  •  Schedule automatic full discoveries
  •  Use the discovery collector
  •  Build and use discovery filters
  •  Troubleshoot discovery issues
  •  Build network partition views
  •  Use the Network Health Dashboard
  •  Create custom dashboards
  •  View device link status and capacity information
  •  Manually instantiate undiscovered devices and connections.
  •  Use the Hop View and Network Partition view
  •  Create a network view with multiple domains
  •  Configure and customize Network Manager polling behavior
  •  Schedule event-based reports
  •  View asset and discovery reports
  •  Perform stitcher customizations to add custom data to a discovery
  •  Configure adaptive polling
  •  Configure database access
  •  Configure a custom report
  •  Schedule a report snapshot

Audience

This course is for administrators, integrators, and users who are responsible for configuring and using Tivoli Network Manager or Network Operations Insight.

Prerequisites

Before taking this course, you should have the following skills: -

  • Basic Linux shell script editing using vi or gedit
  • Understanding of the function of routers and switches and layers 2 and 3 of the Open Systems Interconnect (OSI) model
  • Understanding of the types of devices that operate at Layer 1 of the OSI model

Programme

Introduction and Architecture

  • Features overview
  • Architectural overview
  • Troubleshooting with log and trace files
  • Architectural considerations

 

Discovery Basics

  • How discovery works
  • The discovery wizard
  • Starting discovery
  • Checking discovery status
  • Discovery configuration tabs

 

Advanced Discovery Options

  • Configure discovery of multicast networks
  • Discovery filtering
  • Discovering with collectors
  • Troubleshooting discovery
  • Optimizing discovery

 

Visualization Basics

  • Visualization architecture
  • Event views
  • The Hop View
  • Network views
  • Link status and capacity
  • Tabular and Grid views
  • Tools

 

Advanced Visualization

  • Path Views
  • Topology Editor
  • Device Structure Browser
  • Bookmarks
  • Adding classes and icons
  • Cross-domain network views
  • Network Health Dashboard
  • Create custom dashboards

 

Polling

  • Polling architecture
  • Polling policies
  • Polling definitions
  • Manage and unmanage devices and interfaces
  • Configure adaptive polling
  • Realtime MIB graphing
  • Distributed polling
  • Troubleshooting information

 

Optical Transport and Radio Access Networks

 

Understanding DNCIM

  • DNCIM database basics
  • Populating DNCIM database
  • Mapping information into the MODEL service

 

Customizing Discovery

  • Discovery in-depth
  • Creating database tables
  • Prepare stitchers to enrich discovery
  • Run the custom scripts and stitchers

 

Gateway and Network Fault Isolation

  • Architecture and basis concepts
  • RCA overview
  • Gateway plug-ins
  • New rules for special events
  • Troubleshooting gateway event processing

 

Administrative Perl Scripts

 

Tivoli Network Manager Failover

  • Failover basics
  • What happens with failover

 

Tivoli Network Manager Reports

  • Overview
  • Viewing and scheduling reports
  • Cognos and BIRT reports
  • Included reports
  • Installing Tivoli Common Reporting
  • Troubleshooting Cognos

 

Installing Tivoli Network Manager 4.1.1

  • Installation preparation
  • Installing Tivoli Network Manager
  • The root user post installation tasks
  • Install Tivoli Common Reporting
  • Component communications
  • Optional configuration of OMNIbus processes running as a non-root user
  • Process control
  • Starting Tivoli Network Manager

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:

http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates