Arrow Education reçoit la certification QUALIOPI
La certification QUALIOPI permet à nos clients de faire financer les formations de leurs collaborateurs par les organismes financeurs.
CODE: TK263G
DURÉE: 24 Hours (3 Jours)
PRIX H.T.: €2 100,00
This is an instructor-led course that provides basic introduction of the IBM Security Admin ISPF interface for customers who administer RACF profiles and generate basic RACF overview reports.
This course focuses on frequently used administrative functions, standard reports, and verification functions of IBM Security zSecure Admin. Gain experience in administering RACF profiles using the built-in functions and line commands that the ISPF interface provides. Learn how to report and review RACF profiles using the built-in functions and provided line commands. Verification functions that report RACF database inconsistencies are explored and demonstrated. The CKGRACF function is also described. Finally, you also learn how to produce customized reports, tailor the RACF installation data field, and define company-specific custom fields.
This basic-level course is intended for RACF administrators who use the IBM Security zSecure Admin ISPF panel interface. It is also suitable for RACF administrators, auditors, and compliance officers who use the IBM Security zSecure Admin ISPF panel interface, the built-in functions and commands to review and report about RACF profiles.
Before taking this course, make sure that you have a working knowledge of RACF. It is also recommended you have the following skills:
These skills can be obtained by attending one or more of the following courses:
Unit 1: Run IBM Security zSecure Admin
Unit 2: Select and display existing RACF profiles
Unit 3: Perform profile maintenance
Unit 4: Use Advanced options
Unit 5: Produce RACF administration reports
Unit 6: Create specific user ID and group reports
Unit 7: Create resource reports
Unit 8: Produce RACF management reports
Unit 9: Create customized reports
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show:
The current GTP list price
The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.