Training Offering

IBM System z Hardware Management Console (HMC) Operations

Information

Price £1,190 before tax
Length: 2 Days
Course code: ES24G
Delivery Type Classroom

Session dates

See sessions for other countries
Date Location
  • London (Arrow)
    £1,190 before tax
This training is also available as onsite training. Feel free to contact us for more information.

Description

This course teaches you navigation, operation, and recovery techniques for the Hardware Management Console (HMC) in the System z environment. Through lecture and hands-on exercises, you learn setup and operating procedures for the HMC, gain in-depth problem determination skills, practice HMC operations, and utilize recovery capabilities provided by the System z servers.

Objectives

Identify the zEnterprise 196 and 114, System z10, System z9, and zSeries servers



Describe the major differences of the function and features between the System z servers



Describe and explain the concept of logical partitioning



Identify how various resources are assigned to LPARs during initialization



Describe the functions provided by the HMC and SE




  • User interface styles, local and remote connectivity



Identify HMC home page to log on HMC application



Use the classic UI to:




  • Log on and log off

  • Open objects

  • Navigate the HMC workplace using various selection techniques

  • Exit a task on a window

  • View the online books and use the Help functions

  • Identify the different types of groups

    • CPC group, control hardware

    • Images group, control operating system



  • Build new CPC and images groups

  • Identify the contents of the Details window and determine object status

  • Identify the various task lists



Use the tree UI to:




  • Log on and log off

  • Open objects

  • Navigate the HMC workplace using various selection techniques

  • Exit a task on a panel

  • View the online books and use the Help functions

  • Identify the different types of groups

    • CPC group, control hardware

    • Images group, control operating system



  • Build new CPC and images groups

  • Identify the contents of the Details window and determine object status

  • Identify the various task lists



Describe how exceptions are reported and presented on the HMC using the tree or classic UI



Use the HMC to determine the type and cause of the exception



Describe the three types of hardware messages that can surface on the HMC



Use the HMC to determine the cause of the hardware message



Retrieve the hardware messages from the log



Use the HMC Operating System Messages task to display and send messages to the operating system



Describe the functions that require the use of the access administrator ID



Use the HMC to perform access administrator related tasks



Describe the purpose, functions, and use of the different types of activation profiles




  • Reset profile

  • Image profile

  • Group profile

  • Load profile



Use the HMC to build new profiles, modify, view, or delete existing ones



Use the HMC to determine or change profile assignments Provide operational recommendations for HMC user settings



Use the HMC to perform




  • A manual load operation

  • A system reset

  • Problem determination for a load failure



Invoke the system activity display and describe its purpose



Establish an HMC/SE session using the Single Object Operations task



Identify the difference between the HMC and SE workplace



Navigate using classic or tree UI to Identify CP, channel, and CHPID status for the physical CPC and all LPs



Identify the entry point for I/O and Channel Problem Determination panels



Log off from a CPC session

Participants

This intermediate course is for operations personnel and technical staff who are directly involved in the installation, operation, systems support, and software support of their System z mainframe environment.

Prerequisite(s)

You should have an understanding of:




  • Basic data processing and I/O concepts and terminology

  • z/OS console operation, including display of device, job, and console status

Programme

Day 1

  • Welcome
  • Unit 1: IBM mainframe server hardware: Overview
  • Unit 2: Using the HMC classic style user interface
  • Unit 3: Using the HMC tree style user interface
  • Unit 4: Using the HMC to monitor System z servers
  • Supporting labs

Day 2

  • Review
  • Unit 5: Activation profiles and operational tasks
  • Unit 6: Single object operation: CPC session Supporting labs

Course type

Roadmaps that reference this course are:



•    z/OS Operation and Parallel Sysplex

•    z/OS Operation and Parallel Sysplex

•    z/OS Installation, Tuning, JES, and REXX Programming and Problem Diagnosis


© 2020 Systems Assurance - Arrow ECS. All rights reserved.