CODE: F5N_BIG-DNS-I
LENGTH: 16 Hours (2 days)
PRICE: £1,595.00
Learn how to configure and deploy BIG-IP DNS as it is commonly used. Learn how the Domain Name System (DNS) resolves hostnames into IP addresses, and how to use DNS Express to cache DNS query responses, accelerating DNS resolution. Practice working with key features to perform intelligent DNS resolution and configure wide IP pools to use a path load balancing method. Explore using persistence to effectively return one or more clients to the same virtual server on each query. Practice manual controls for resuming certain load balancing behaviors in the event of an outage. Configure BIG-IP DNS to participate in the DNSSEC chain of trust. Configure limit settings on virtual servers, and wide IP pools to temporarily direct client traffic away from resources that may not be performing at certain thresholds of efficiency. Customize intelligent DNS resolution using iRules on a wide IP. Learn how to configure a BIG-IP DNS sync group.
Reinforce knowledge transfer through the use of hands-on labs, and gain the confidence needed to start using BIG-IP DNS in a production environment.
Upon successful completion of this course, the student will be able to:
This course is intended for system and network administrators responsible for installation, setup, configuration, and administration of BIG-IP DNS systems.
The following free Self-Directed Training (SDT) courses, although optional, are helpful for any student with limited BIG-IP administration and configuration experience:
• Getting Started with BIG-IP
• Getting Started with BIG-IP DNS
General network technology knowledge and experience are recommended before attending any F5 Global Training Services instructor-led course, including OSI model encapsulation, routing and switching, Ethernet and ARP, TCP/IP concepts, IP addressing and subnetting, NAT and private IP addressing, NAT and private IP addressing, default gateway, network firewalls, and LAN vs. WAN.
The following course-specific knowledge and experience is suggested before attending this course:
• DNS resolution process
• Experience configuring DNS content and resolution servers
• DNSSEC
Chapter 1: Setting Up the BIG-IP System
• Introducing the BIG-IP System
• Initially Setting Up the BIG-IP System
• Archiving the BIG-IP Configuration
• Leveraging F5 Support Resources and Tools
Chapter 2: Introducing the Domain Name System (DNS) and BIG-IP DNS
• Understanding the Domain Name System (DNS)
• Reviewing the Name Resolution Process
• Implementing BIG-IP DNS
• Using DNS Resolution Diagnostic Tools
Chapter 3: Accelerating DNS Resolution
• Introducing DNS Resolution with BIG-IP DNS
• BIG-IP DNS Resolution Decision Flow
• Configuring BIG-IP DNS Listeners
• Resolving DNS Queries in the Labs (Lab Zone Records)
• Load Balancing Queries to a DNS Server Pool
• Accelerating DNS Resolution with DNS Cache
• Accelerating DNS Resolution with DNS Express
• Introducing Wide IPs
• Using Other Resolution Methods with BIG-IP DNS
• Integrating BIG-IP DNS into Existing DNS Environments
Chapter 4: Implementing Intelligent DNS Resolutions
• Introducing Intelligent DNS Resolution
• Identifying Physical Network Components
• Identifying Logical Network Components
• Collecting Metrics for Intelligent Resolution
• Configuring Data Centers
• Configuring a BIG-IP DNS System as a Server
• Configuring a BIG-IP LTM System as a Server
• Establishing iQuery Communication between BIG-IP Systems
• Configuring a Non-F5 Server
• Defining Links and Routers
• Configuring Wide IP Pools
• Configuring Wide IPs
• Managing Object Status and State
• Using the Traffic Management Shell (TMSH)
Chapter 5: Using LDNS Probes and Metrics
• Introducing LDNS Probes and Metrics
• Types of LDNS Probes
• Excluding an LDNS from Probing
• Configuring Probe Metrics Collection
Chapter 6: Load Balancing Intelligent DNS Resolution
• Introducing Load Balancing on BIG-IP DNS
• Using Static Load Balancing Methods
• Round Robin
• Ratio
• Global Availability
• Static Persist
• Other Static Load Balancing Methods
• Using Dynamic Load Balancing Methods
• Round Trip Time
• Completion Rate
• CPU
• Hops
• Least Connections
• Packet Rate
• Kilobytes per Second
• Other Dynamic Load Balancing Methods
• Using Quality of Service Load Balancing
• Persisting DNS Query Responses
• Configuring GSLB Load Balancing Decision Logs
• Using Manual Resume
• Using Topology Load Balancing
Chapter 7: Monitoring Intelligent DNS Resources
• Exploring Monitors
• Configuring Monitors
• Assigning Monitors to Resources
• Monitoring Best Practices
Chapter 8: Advanced BIG-IP DNS Topics
• Implementing DNSSEC
• Setting Limits for Resource Availability
• Using iRules with Wide IPs
• Introducing Other Wide IP Types
• Implementing BIG-IP DNS Sync Groups
F5N_BIG-LTM-CFG-3, Configuring BIG-IP LTM: Local Traffic Manager v.16.1
F5N_BIG-AWF-CFG, Configuring F5 Advanced WAF (previously licensed as ASM) v.16.1
F5N_BIG-EGW-APM, Configuring BIG-IP APM: Access Policy Manager v.16.1
Exam 302 – BIG-IP DNS Specialist
Prerequisites: Valid F5-CA, BIG-IP Certification
Candidates that pass Exam 302 will receive the F5 Certified! Technology Specialist, BIG-IP DNS certification.
People with this certification have the fundamental knowledge necessary to application delivery architects and application delivery engineers working with BIG-IP DNS, including the ability to understand the basic operation of the DNS protocol, deploy and test configurations, and troubleshoot and remedy common misconfigurations.
These individuals also are able to explain the capabilities of DNS services to deploy applications globally.
Receiving the F5-CTS, BIG-IP DNS certification is a prerequisite for the Cloud Solutions Expert certification tracks.
View Exam 302 study materials on AskF5
Exam vouchers can be purchased from Arrow ECS at an additional charge. Vouchers can be used at
www.vue.com/f5 to schedule exams at a time and location convenient to the attendee.
Course Changes since v15
The Configuring DNS v16.1 course presents much of the same content as v15.1, with very minor modifications.