Arrow Electronics, Inc.

Power Systems for AIX IV: Performance Management

CODE: AN51G

LENGTH: 40 Hours (5 days)

PRICE: $4,000.00

Description

Develop the skills to measure, analyze, and tune common performance issues on IBM Power Systems running AIX.

Learn about performance management concepts and techniques and how to use the basic AIX tools to monitor, analyze, and tune an AIX system. The course covers how virtualization technologies such as the PowerVM environment and workload partitions affect AIX performance management. Monitoring and analyzing tools discussed in this course include vmstat, iostat, sar, tprof, svmon, netstat, lvmstat, and topas. Tuning tools include schedo, vmo, ioo, no, and nfso.

The course also covers how to use Performance Problem Reporting (PerfPMR) to capture a variety of performance data for later analysis.

Each lecture is reinforced with extensive hands-on lab exercises which provide practical experience.

The materials include AIX 7.1 enhancements and the exercises are executed on a POWER8 lab environment.

Objectives

  • Define performance terminology
  • Describe the methodology for tuning a system
  • Identify the set of basic AIX tools to monitor, analyze, and tune a system
  • Use AIX tools to determine common bottlenecks in the central processing unit (CPU), virtual memory manager (VMM), logical volume manager (LVM), internal disk input/output (I/O), and network subsystems
  • Use AIX tools to demonstrate techniques to tune the subsystems

Audience

This advanced course is for:

  • AIX technical support personnel
  • Performance benchmarking personnel
  • AIX system administrators

Prerequisites

You are expected to have basic AIX system administration skills. These skills can be obtained by attending the following courses:

  • AIX Jumpstart for UNIX professionals (AN14G) or
  • Power Systems for AIX II: Implementation and Administration (AN12G)

It is very helpful to have a strong background in TCP/IP networking to support the network performance portion of the course. These skills can be built or reinforced by attending:

  • TCP/IP for AIX Administrators (AN21G)

It is also very helpful to have a strong background in PowerVM (particularly micro partitioning and the role of the Virtual I/O Server). These skills can be built or reinforced by attending:

  • Power Systems for AIX - Virtualization I: Implementing Virtualization (AN30G)

Programme

Day 1

  • Unit 1 - Performance analysis and tuning overview
  • Exercise 1 - Working with tunable files Unit 2 - Data collection
  • Exercise 2 - Data collection
  • Unit 3 - Monitoring, analyzing, and tuning CPU usage
  • Exercise 3 - Monitoring, analyzing, and tuning CPU usage (parts 1 and 2)

Day 2

  • Exercise 3 - Monitoring, analyzing, and tuning CPU usage (parts 3, 4 and 5)
  • Unit 4 - Virtual memory performance monitoring and tuning Exercise 4 - Virtual memory performance monitoring and tuning Student’s choice optional exercise from exercise 3 or exercise 4

Day 3

  • Unit 5 - Physical and logical volume performance
  • Exercise 5 - Physical and logical volume performance
  • Unit 6 - File system performance monitoring and tuning (topic 1)
  • Exercise 6 - File system performance monitoring and tuning (parts 1, 2, and 3)

Day 4

  • Unit 6 - File system performance monitoring and tuning (topic 2)
  • Exercise 6 - File system performance monitoring and tuning (part 4) Unit 7 - Network performance
  • Exercise 7 - Network performance
  • Student's choice optional exercise from exercises 3, 4, or 6

Day 5

  • Unit 8 - NFS performance
  • Exercise 8 - NFS performance tuning
  • Unit 9 - Performance management methodology Exercise 9 - Summary exercise
  • Student's choice optional exercises from exercises 3, 4, 6, or 7

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates