Arrow Electronics, Inc.

IBM System z Parallel Sysplex Operations

CODE: ES73G

LENGTH: 24 Hours (3 days)

PRICE: $2,795.00

Description

This course is designed so that students can learn how z/OS systems operate in a Parallel Sysplex environment through discussion topics and hands-on lab exercises. Students learn problem determination skills, practice enhanced sysplex operations, including management of the coupling facility (CF), and use recovery capabilities provided by the System z servers.

The course consists of six units and 12 hands-on lab exercises.

Objectives

  • Describe common sysplex terminology, concepts, and benefits provided by a Parallel Sysplex configuration
  • Identify the basic hardware and software components that make up the Parallel Sysplex environment and how they are used
  • Use z/OS MVS commands to identify XCF signaling and sysplex shared couple data set usage and to determine current operational status
  • Describe CF operation; how and when the CFCC is loaded on a System z LPAR, the various CF link definitions and how they can be used
  • Identify CF structure types, definition and allocation process, and how they are used in the CF
  • Use z/OS MVS commands to display structure status
  • Use CF operator commands to display and change the operational status of a CF
  • Describe and demonstrate recommended procedures and typical z/OS MVS commands to manage sysplex members, coupling facilities, structure rebuilds, and couple data sets
  • Identify potential problems during system removal, CF structure or CDS usage, and determine appropriate operator action
  • Explain the differences and benefits of having stand-alone CF and internal CF configurations
  • Describe the purpose and use of Sysplex Failure Manager and how SFM can be used to address sympathy sickness
  • Explain why time synchronization is important and how server time protocol is used
  • Describe console usage and mode of operation for a system and a sysplex
  • Describe the IPL sequence and identify where and when sysplex activation is done during IPL
  • Identify key areas with the IPL, explaining potential problems and how to avoid them

Audience

The audience includes operations personnel and technical staff who are directly involved in the installation, operation, systems support, and software support of their Parallel Sysplex environment.

Prerequisites

You should have an understanding of:

  • Basic data processing and I/O concepts and terminology
  • z/OS console operation, including display of device, job, and console status

Programme

Day 1

  • Welcome
  • Unit 1: Sysplex overview
  • Unit 2: Coupling facility
  • Supporting labs

Day 2

  • Review
  • Unit 3: Sysplex operation and recovery
  • Supporting labs

Day 3

  • Review and labs
  • Unit 4: Sysplex Failure Manager
  • Unit 5: Server Time Protocol operation
  • Unit 6: z/OS IPL flow
  • Supporting labs

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.  

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course.  Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates