CODE: ZL1_6F91
LENGTH: 3 dage
PRICE: kr 17.460,00
This course provides students with an understanding of the configurations required to map participants in a supply chain to the corresponding roles in Sterling Order Management. The course also teaches students the process of setting up the Sterling Selling and Fulfillment Foundation business process workflow. This course is primarily designed for developers and implementers.
This course begins with an overview of Sterling Order Management and the business models it supports. The course then describes how to define participants and create organizations and users. Through a combination of procedural information and exercises, students will learn about topics such as how to assign attributes to the different roles defined in Sterling Order Management and configure user access policies.
The course also covers Process Modeling features, including how to set up a business process workflow for an organization. Students are then introduced to statuses, conditions, transactions, and other components of a process type pipeline. The course then describes how to create a process type pipeline.
After completing this course, students should be able to:
Map the participant details to their appropriate roles using Application Platform.
Create users and configure user security features using Application Platform.
Describe Process Modeling.
Create the following components:
Statuses, Conditions, and Services
Events and Event Handlers
Actions and Transactions
Create pipelines and pipeline determination rules.
This course is designed to train developers and implementrs.
None.
The following topics will be covered during this course:
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:
http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show: