Arrow Electronics, Inc.

PowerHA SystemMirror 7 Planning, Implementation, Customization and Basic Administration

CODE: AN61G

LENGTH: 40 Hours (5 dage)

PRICE: kr 29.100,00

Description

This course is designed to prepare students to install and configure a highly available cluster using PowerHA SystemMirror.

Objectives

  • Explain what high availability is
  • Outline the capabilities of PowerHA SystemMirror
  • Design and plan a highly available PowerHA cluster
  • Install and configure PowerHA SystemMirror in the following modes of operation:
  • Single resource group on a primary node with standby node (active/passive)
  • Two resource groups in a mutual takeover configuration (active/active)
  • Configure resource group startup, fallover, and fallback policies
  • Perform basic system administration tasks for PowerHA
  • Perform basic customization for PowerHA
  • Perform basic problem determination and recovery

This course is the first in the PowerHA 7 curriculum. The following courses can be taken after this course is completed:

  • PowerHA 7 Advanced Configurations (AN62G) 

Audience

The audience for this advanced course is students who are experienced AIX system administrators with TCP/IP networking and AIX Logical Volume Manager (LVM) experience who are responsible for the planning and installation of a PowerHA SystemMirror 7.1 and later cluster on an IBM Power Systems server running AIX V6.1 or later. The lab exercises are conducted on an AIX 7.1 TL2 level system.

Prerequisites

You should be AIX system administrator and have TCP/IP, LVM storage, and disk hardware implementation skills. These skills are addressed in the following courses or can be obtained through equivalent education and experience:

  • Power Systems for AIX II:  AIX Implementation and Administration (AN12G)

Programme

Day 1

  • Welcome and course introduction
  • Unit 1: Introduction to PowerHA SystemMirror
  • Unit 2: Planning and configuring network and storage for PowerHA SystemMirror
  • Exercise 1: Lab setup, cluster planning, and exploring fallover
  • Exercise 2: Preparing the AIX environment for PowerHA SystemMirror

Day 2

  • Unit 3: Configuring applications for PowerHA SystemMirror
  • Unit 4: Configuring a PowerHA SystemMirror cluster
  • Exercise 3: Preparing an application for integration with SystemMirror
  • Exercise 4: Initial cluster configuration

Day 3

  • Unit 5: Cluster validation and testing
  • Unit 6: Basic PowerHA SystemMirror administration
  • Exercise 5: Cluster validation and testing
  • Exercise 6: Extending the configuration

Day 4

  • Unit 7: Events
  • Unit 8: Basic troubleshooting
  • Exercise 7: Events
  • Exercise 8: PowerHA SystemMirror problem determination

Day 5

  • Unit 9: PowerHA SystemMirror installation
  • Exercise 9: Install and maintain PowerHA SystemMirror
  • Open lab

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

10 jul 2023

Virtual Classroom (GMT / UTC)

BST

English

Instructor Led Online

kr 29.100,00

We also offer sessions in other countries