Arrow Electronics, Inc.

Hardware Configuration and Definition (HCD) for z/OS

CODE: ES96G

LENGTH: 32 Hours (4 dage)

PRICE: kr 23.280,00

Description

Learn to work with the Hardware Configuration Definition (HCD) function for z/OS, and to plan and initiate dynamic reconfiguration of your zSeries hardware environment. Learn to use the HCD dialogs of z/OS to create an Input/Output (I/O) configuration and dynamically alter the I/O configuration. Learn about the creation of an I/O Configuration Dataset (IOCDS) and various reports that HCD can build. Use a z/OS system to reinforce lecture topics and to practice working with the HCD dialogs. Hands-on lab projects may be done in teams depending on the number of attendees and location.

Objectives

  • Describe new zSeries processor technology
  • Code new zSeries processors (z9 to z196)
  • Code FICON channels and FICON CTCs
  • Code Coupling Facilities (CF) and CF links
  • Code cascaded FICON Directors
  • Create an IODF work file on a z processor from scratch
  • Use CHPID mapping tool to create a validated work IODF
  • Use work IODF and create a production IODF
  • Perform Dynamic I/O changes on a real z/OS system
  • Build a LOADxx parmlib member for initial program load (IPL)
  • View configuration graphically
  • Create appropriate configuration reports

Audience

This course is for people who are responsible for maintaining the I/O configuration contained in the input/output data files (IODFs) and input/output configuration data sets (IOCDs) at their z/OS installation.

Prerequisites

You should have:

  • A basic knowledge of z/OS and I/O configuration

This knowledge can be developed on the job, or by taking Fundamental System Skills in z/OS (ES10A).

Programme

Day 1

  • Welcome
  • Unit 1: HCD introduction
  • Unit 2: IOCP and MVSCP macro review
  • Unit 3: HCD dialog
  • Unit 4: LPAR and logical control unit concepts
  • Unit 5: OSAs, OSA/ICC and HiperSockets
  • Unit 6: Review of zSeries hardware
  • Exercise 1: Overview of lab environment
  • Exercise 2: HCD familiarity

Day 2

  • Unit 7: zSeries I/O architecture: Logical channel subsystems
  • Unit 8: Advanced DASD concepts: EAV/PAV and multiple subchannel sets
  • Unit 9: FICON, FICON CTCs, and FICON directors
  • Exercise 3: Coding a zSeries 2817
  • Exercise 4: Adding FICON directors to your configuration (optional)
  • Exercise 5: Incremental migration from IOCP deck (optional)

Day 3

  • Unit 10: HCD implementation and migration
  • Unit 11: IPL and LOADxx member
  • Unit 12: Dynamic I/O reconfiguration
  • Unit 13: z196 HCD and using CMT
  • Exercise 6: Building a LOADxx member
  • Exercise 7: Perform dynamic I/O

Day 4

  • Unit 14: FICON CTCs for sysplex
  • Unit 15: HCD and Parallel Sysplex
  • Exercise 8: Coding a 2817 using the CMT
  • Exercise 9: Coding CF coupling links
  • Exercise 10: Coding sysplex FICON CTCs

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.  

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course.  Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates