Arrow Electronics, Inc.

BMC Course for Control-M 21.x: Advanced Administering

CODE: BMC_AUTO-CMAD-9212

DURÉE: 24 Hours (3 Jours)

PRIX H.T.: €2 880,00

Description

This course provides Administrators and Consultants with the theory and hands-on experience to install additional components and perform advanced tasks that are beyond everyday administration, which will help to secure and fine tune the Control-M environment. This instructor-led training covers advanced tasks administrators are required to perform in Control-M such as ControlM Migration, Distributed Control-M/Enterprise Manager, Workload Archiving, Role-Based Administration, Remote Host with SSH, Administering Control-M using Automation API, Secure Sockets Layer (SSL) Configuration, and Housekeeping Activities.

Objectifs

  • Migrate Control-M/Enterprise Manager
  • Migrate Control-M/Server
  • Install Distributed Control-M/Enterprise Manager
  • Describe Control-M Workload Archiving
  • Install Control-M Workload Archiving
  • Configure Control-M Workload Archiving Policies
  • Configure Control-M Workload Archiving Disk Space and Cleanup Settings
  • Explain the purpose of the Control-M Automation API
  • Install the Control-M Automation API and Automation API Command Line Interface
  • Use the Environment, Session, Authentication, Config, Provision, Usage Automation API Services and Control M JSON files
  • Generate Self Signed Certificates
  • Configure SSL in Zones 1, 2 and 3
  • Configure SSL with LDAP
  • Perform health checking tasks for Control-M
  • Monitor Control-M processes

Programme

Module 1: Control-M Migration

 

  • Describe the BMC AMIGO Program
  • Describe the Control-M/Enterprise Manager and Control-M/Server migration considerations and process
  • Export/import the Control-M/Enterprise Manager data between environments
  • Migrate Control-M/Server data manually or automatically
  • Migrate Control-M Workload Archiving
  • Implement post-Control-M/Server migration procedures
  • Rename the Control-M/Server
  • Connect the Gateway to the new Control-M/Server

 

Module 2: Additional Distributed Control-M Enterprise Manager Installation

 

  • Describe Distributed Control-M/EM
  • Explain the use cases for Distributed Control-M/EMs
  • List the compatible hardware and operating systems for a Distributed Control-M/EM
  • Implement the Control-M/EM pre-installation steps
  • Install a Distributed Control-M/EM
  • Connect a load balancer to the Control-M/EM servers
  • Configure a HostPort for each EM server component when there is a firewall in the environment

 

Module 3: Control-M Workload Archiving

 

  • Describe Control-M Workload Archiving and its purpose
  • Explain the Control-M Workload Archiving installation process
  • List the Control-M Workload Archiving installation prerequisites
  • Install Control-M Workload Archiving
  • Configure Control-M Workload Archiving Policies
  • Configure Control-M Disk Space and Cleanup Settings
  • Configure Workload Archiving System Parameters
  • Perform an Archive Search

 

Module 4: Role-based Administration

 

  • Overview of Role-Based Administration
  • Assigning Role-Based Administration

 

Module 5: Administering Control-M Using Automation API

 

  • Describe Control-M Automation API
  • Explain how Control-M Automation API can be used to administer the Control-M environment
  • List the prerequisites steps for getting started with the Control-M Automation API
  • Install the required Automation API components
  • Access the Automation API Documentation
  • Identify and describe the Control-M Automation API Services
  • Use the following Control-M Automation API Services Environment, Session, Authentication
  • Understand how Control-M JSON is written and why it is used

 

Module 6: Using the Automation API Config Service

 

  • Use the Config Service to configure the Control-M environment

 

Module 7: Using Automation API Provision and Usage Services

 

  • Use the Provision Service to:

- Install, uninstall, upgrade, downgrade and configure Control-M/Agents and Application Plug-ins

- Install, configure and uninstall Control

  • Use the Usage Service to generate a task usage report

 

Module 8: SSL Configuration

 

  • Generate certificates (both your own and self
  • Describe the Zones 1, 2 and 3 SSL configuration processes
  • Configure and enable SSL on the Control-M Web Server (Zone 1)
  • Configure and enable SSL in Zones 2 and 3
  • Disable SSL on Control-M components
  • Configure SSL with LDAP

 

Module 9: Control-M Health Checking

 

  • Explain the Control-M Health Check process
  • Implement Control-M process monitoring
  • Identify key Control-M log files to parse for errors
  • Examine the Control-M/Agent daily log
  • Review and implement Control-M housekeeping jobs
  • Implement a Control-M log file system cleanup process
  • Review and implement Control-M performance tuning parameters
  • Implement Control-M performance monitoring

Follow on courses

Recommended Trainings

 

  • Control-M 21.x: Fundamentals Using (WBT)
  • Control-M 21.x: Fundamentals Operating (ILT/ASP)
  • Control-M 21.x: Fundamentals Administering (ILT/ASP)

Test et Certification

 

Dates de session