Arrow Education reçoit la certification QUALIOPI
La certification QUALIOPI permet à nos clients de faire financer les formations de leurs collaborateurs par les organismes financeurs.
CODE: ZL1_OE98
DURÉE: 1 Jours
PRIX H.T.: €780,00
In this classroom course, you will learn basic concepts and skills you need to be productive users on Power Systems with IBM i. With plenty of hands-on lab exercises, we show everything from signing onto the available user interfaces; green screen environment and IBM Navigator for i.
You will learn how objects are managed on the system and how you display these objects. You will learn to use control language (CL) commands (fast path) and how to work with and manage messages on the system. Students will also learn how to the system manages work and how you manage your printouts. Lastly, students will also get a basic overview of security.
After completing this course, you should be able to:
•Explain the functions supported by IBM i operating systems
•Explain Power System with IBM i models and generations
•Explain which applications are supported
•Sign on / off the system
•Use the display station keyboard
•Use the online help that is available
•Use the different interfaces available for IBM i
•Understand how objects are managed
•Enter control language (CL) commands
•Send and receive messages and work with message queues
•Manage work and output
•Explain basic security concepts on IBM i
This course is intended for new users employed in a data processing environment who are new to Power Systems with IBM i.
Cours magistral sans travaux pratiques
There are no prerequisites for this course.
Welcome
Unit 1 - Introduction and overview to IBM i
Unit 2 - Using the 5250 emulation interface
Exercise 1- Using the 5250 emulation interface
Unit 3 – Overview of IBM I Access Client Solutions
Exercise 2 – Overview of IBM i Access Client Solutions
Unit 4 - Using IBM Navigator for i
Exercise 3 - Using IBM Navigator for i
Unit 5 - Using the messages function on IBM i
Exercise 4 - Using the messages function with a display session
Exercise 5 - Using the messages function with IBM Navigator for i
Unit 6 - Using CL commands on IBM i
Exercise 6 - Using CL commands with a display session
Exercise 7 - Using CL commands with IBM Navigator for i
Unit 7 - Managing objects on IBM i
Exercise 8 - Object management on IBM i
Unit 8 - Managing your work on IBM i
Exercise 9 - Tracking jobs and printouts on IBM i
Unit 9 - IBM i security overview
Unit 10 - Additional education
0
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show:
The current GTP list price
The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.