Arrow Education reçoit la certification QUALIOPI
La certification QUALIOPI permet à nos clients de faire financer les formations de leurs collaborateurs par les organismes financeurs.
CODE: ZL1_TM405
DURÉE: 4 Jours
PRIX H.T.: €3 180,00
In this instructor-led course, you learn how to manage batch workloads in z/OS with IBM Tivoli Workload Scheduler for z/OS. During the course, you use ISPF panels to create scheduling definitions and perform operational tasks. There is also a brief overview of the end-to-end environment. The course covers creating and controlling planning objects, such as workstations, applications, calendars, and resources. You learn how to schedule these objects into a daily planning cycle and then monitor and manage them. This training class is provided in a classroom environment with multiple opportunities for hands-on lab practice. The scenarios used in this class are based on IBM Tivoli Workload Scheduler for z/OS version 9.2.0.
After you complete this course, you can perform the following tasks:
This course is intended for schedulers and operators who will schedule and manage jobs in a z/OS environment using IBM Tivoli Workload Scheduler for z/OS 9.2.0.
Before taking this course, you should have the following skills:
Introduction
Workstations
Calendars, periods, and run cycle groups
Applications
Operation submission, throughput, and monitoring
Long-term and current plans
Restart and cleanup
Special resources
Automated job tailoring
Automatic recovery
Managing unplanned work
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show:
The current GTP list price
The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.