Arrow Education reçoit la certification QUALIOPI
La certification QUALIOPI permet à nos clients de faire financer les formations de leurs collaborateurs par les organismes financeurs.
CODE: ZL1_WE761
DURÉE: 4 Jours
PRIX H.T.: €2 995,00
This course is also available as self-paced virtual (e-learning) course Administration of IBM DataPower Gateway V7.6 (ZE761G). This option does not require any travel.
IBM DataPower Gateway Appliances are network devices that help secure, integrate, and optimize access to web, web services, mobile, and API workloads. Through instructor-led lectures and hands-on lab exercises, you learn how to run various administrative procedures, from initial installation and setup through ongoing maintenance of the appliances in production. You learn about the available management interfaces, such as the command-line interface (CLI), Web Management graphical interface, and XML Management Interface. You also learn how to use these interfaces to run various administrative tasks, such as upgrading firmware, running backup and restore operations, and configuring user accounts and domains. The course includes some information on upgrading firmware and working with DataPower hardware appliances.
This course exercises uses the following appliances:
Information in the course units also applies to other DataPower appliances.
The lab environment for this course uses the Ubuntu Linux Operating System on an ESX image that runs on the IBM Remote Lab Platform.
For information about other related courses, see the IBM Training website:
ibm.com/training
This course is designed for administrators who install, manage, and monitor IBM DataPower Gateway Appliances. The course is also relevant for developers who administer appliances.
You should successfully complete Technical Introduction to IBM WebSphere DataPower Gateway Appliances V7 (VW700G, no longer available).
You should also be familiar with:
Course introduction
DataPower deployment environments
Initial setup
Managing firmware
Exercise: Upgrading image firmware
DataPower administration overview
Using CLI and the XML Management Interface to configure appliance access
Exercise: Using the CLI and the XML Management Interface to manage DataPower appliances
DataPower services overview
Using the Web Management Blueprint Console to configure appliance access
Troubleshooting
Exercise: Using the troubleshooting tools to debug errors
DataPower cryptographic tools and SSL setup
Exercise: Securing connections with SSL
Logging and log targets
Exercise: Logging to an external system
Course summary
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show:
The current GTP list price
The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.