Arrow Electronics, Inc.

Power Systems for AIX - PowerVM I Implementing Virtualization

CODE: AN30G

LENGTH: 40 Hours (5 days)

PRICE: €3.900,00

Description

This course provides an overview of the PowerVM edition's features on POWER processor-based systems. It explains the new features and benefits of virtualization including processor virtualization, Virtual I/O Server, and virtual devices, such as virtual Ethernet, virtual SCSI, and virtual Fibre Channel adapters. Basic and advanced configurations of the Virtual I/O Server and its clients are discussed including various availability options.

Expand your knowledge about PowerVM features that were introduced in Power Systems for AIX I: LPAR Configuration and Planning (AN11G).

This course provides lectures and hands on labs in an instructor lead course environment, either in a face-to-face classroom or in a live virtual classroom environment (ILO - Instructor Led Online).

Objectives

  • Configure virtual SCSI devices that are backed by physical volumes, logical volumes, and optical media devices 
  • Configure the Optical Media Repository, load a CD image, and use it to install a new AIX partition
  • Configure virtual Fibre channel devices using NPIV technology
  • Configure Ethernet link aggregation for load balancing and backup channel in the VIOS
  • Configure Shared Ethernet adapter failover and load sharing
  • Configure vNIC failover
  • Perform Virtual I/O Server maintenance operations

Audience

This advanced course is appropriate for System Administrators, Technical Support Personnel, and Business Partners responsible for implementing LPARs on IBM Power Systems with AIX servers.

Prerequisites

You must have advanced system administration experience with AIX 6 or AIX 7. This prerequisite can be met by attending one of the following courses:

Power Systems for AIX II: Implementation and Administration (AN12G) 

Power Systems for AIX III: Advanced Administration and Problem Determination (AN15G) 

AIX Jumpstart for UNIX Professionals (AN14G)

Alternatively, you must have equivalent AIX and LPAR skills.

General TCP/IP knowledge is strongly recommended.

You are also expected to have logical partition administration skills on Power Systems servers, which can be obtained by attending Power Systems for AIX I: LPAR Configuration and Planning (AN11G).

Programme

  • Unit 1: Introduction to partitioning
  • Exercise 1: Power Systems documentation overview
  • Unit 2: HMC V8 enhancements
  • Exercise 2: HMC enhanced interface
  • Unit 3: Processor virtualization
  • Exercise 3: Processor virtualization configuration
  • Unit 4: Virtual Ethernet
  • Exercise 4: Virtual Ethernet adapter configuration
  • Unit 5: Virtual I/O Server and Shared Ethernet Adapter
  • Exercise 5: Virtual I/O Server configuration
  • Unit 6: Virtual SCSI devices
  • Exercise 6: Client partition configuration
  • Unit 7: Virtual network configuration with dual VIOS
  • Exercise 7: SEA failover setup
  • Unit 8: Virtual SCSI configurations with dual VIOS
  • Exercise 8: Dual VIO server configuration with MPIO in the client partition
  • Unit 9: Virtual Fibre Channel devices
  • Exercise 9: Virtual Fibre Channel adapter configuration
  • Unit 10: HMC Service Management
  • Exercise 10: Manage service events
  • Unit 11: PowerVM advanced systems maintenance
  • Exercise 11: PowerVM system maintenance
  • Exercise 12: (Optional) File-backed virtual SCSI devices

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

15 mei 2023

Virtual Classroom (GMT / UTC)

BST

English

Instructor Led Online

€ 3.900,00 € 3.510,00

16 mei 2023

Virtual Classroom (GMT / UTC)

BST

English

Instructor Led Online

€ 3.900,00 € 3.510,00

We also offer sessions in other countries