CODE: F5N_BIGIPAD_LTM_BDLE
LENGTH: 40 Hours (5 days)
PRICE: €3.850,00
Administering BIG-IP v16.1
This 2-day course gives network administrators, network operators, and network engineers a functional understanding of the BIG-IP system as it is commonly deployed in an application delivery network.
The course introduces students to the BIG-IP system, its configuration objects, how it processes traffic, and how typical administrative and operational activities are performed.
The course includes lecture, hands-on labs, interactive demonstrations, and discussions.
Topics covered:
Configuring BIG-IP LTM v16.1: Local Traffic Manager
This 3-day course gives network professionals a functional understanding of BIG-IP Local Traffic Manager, introducing students to both commonly used and advanced BIG-IP LTM features and functionality.
Incorporating lecture, extensive hands-on labs, and classroom discussion, the course helps students build the well-rounded skill set needed to manage BIG-IP LTM systems as part of a flexible and high performance application delivery network.
Topics covered:
At the end of this course, the student will be able to:
Administering BIG-IP v16.1
Configuring BIG-IP LTM v16.1: Local Traffic Manager
This course is intended for system and network administrators, operators, and engineers responsible for managing the normal day-to-day operation and administration of a BIG-IP application delivery network, and installation, setup, configuration, and administration of the BIG-IP LTM system.
The following free web-based training courses, although optional, will be very helpful for any student with limited BIG-IP administration and configuration experience. These courses are available at LearnF5 (https://www.f5.com/services/training):
• Getting Started with BIG-IP
• Getting Started with BIG-IP Local Traffic Manager (LTM) web-based training
The following general network technology knowledge and experience are recommended before attending any F5 Global Training Services instructor-led course:
• OSI model encapsulation
• Routing and switching
• Ethernet and ARP
• TCP/IP concepts
• IP addressing and subnetting
• NAT and private IP addressing
• Default gateway
• Network firewalls
• LAN vs. WAN
Administering BIG-IP v16.1
Chapter 1: Setting Up the BIG-IP System
Chapter 2: Traffic Processing Building Blocks
Chapter 3: Using NATs and SNATs
Chapter 4: Monitoring Application Health
Chapter 5: Modifying Traffic Behavior with Profiles
Chapter 6: Modifying Traffic Behavior with Persistence
Chapter 7: Administering the BIG-IP System
Chapter 8: Configuring High Availability
Configuring BIG-IP LTM v16.1: Local Traffic Manager
Chapter 1: Setting Up the BIG-IP System
Chapter 2: Reviewing Local Traffic Configuration
Chapter 3: Load Balancing Traffic with LTM
Chapter 4: Modifying Traffic Behavior with Persistence
Chapter 5: Monitoring Application Health
Chapter 6: Processing Traffic with Virtual Servers
Chapter 7: Processing Traffic with SNATs
Chapter 8: Modifying Traffic Behavior with Profiles
Chapter 9: Selected Topics
Chapter 10: Customizing Application Delivery with iRules
Chapter 11: Customizing Application Delivery with Local Traffic Policies
Chapter 12: Securing Application Delivery with LTM
Chapter 13: Final Lab Project
Chapter 14: Additional Training and Certification
Administering BIG-IP v.16.1
Exam 201 – TMOS Administration
Prerequisite: Valid passing score on Exam 101 or valid F5-CTP, Sales Certification
This is the second and final exam that must be completed successfully by candidates wishing to achieve F5 Certified! Administrator, BIG-IP status.
Passing this exam shows independence in performing day-to-day operations and basic troubleshooting of TMOS-based devices in various application environments after it has been installed, configured, and implemented.
Individuals may choose to complete their certification journey here or move on to pursue the Technical Professional, Technical Specialist, Cloud or Security Solutions certification tracks.
View Exam 201 study materials on AskF5Configuring BIG-IP LTM v16.1: Local Traffic Manager
Exam 301a - BIG-IP LTM Specialist: Architect, Set-up, Deploy
Prerequisites: Valid F5-CA, BIG-IP Certification
This is the first of two exams in the F5 Certified Technology Specialist, BIG-IP LTM certification and serves as a prerequisite to exam 301b.
Candidates who pass this exam possess an understanding of underlying principles – from SSL-based VPN implementation to symmetric and asymmetric acceleration – and can draw on that insight to integrate BIG-IP LTM into existing networks as well as new implementations.
Receiving the F5-CTS, BIG-IP LTM certification is a prerequisite for both the Cloud and Security Solutions Expert certification tracks.
View Exam 301a study materials on AskF5
Exam 301b - BIG-IP LTM Specialist: Maintain and Troubleshoot
Prerequisites: Valid F5-CA, BIG-IP Certification, valid passing score on Exam 301a
This is the second exam candidates are required to pass in order to receive the F5 Certified Technology Specialist, BIGIP LTM certification.
Passing this exam validates their ability to design, implement, maintain, and troubleshoot advanced F5 product features to enhance the effectiveness of an Application Delivery Network.
In addition, it shows that a candidate understands underlying principles – from SSL-based VPN implementation to symmetric and asymmetric acceleration – and can draw on that insight to integrate BIG-IP LTM into existing networks as well as new implementations.
Receiving the F5-CTS, BIG-IP LTM certification is a prerequisite for both the Cloud and Security Solutions
Expert certification tracks.
View Exam 301b study materials on AskF5Exam vouchers can be purchased from Arrow ECS at an additional charge. Vouchers can be used at
www.vue.com/f5 to schedule exams at a time and location convenient to the attendee.
Course Changes since v15
Administering BIG-IP v.16.1
Configuring BIG-IP LTM v16.1: Local Traffic Manager