Arrow Electronics, Inc.

AIX Jumpstart for UNIX Professionals

CODE: AN14G

LENGTH: 40 Hours (5 days)

PRICE: kr39 425,00

Description

Provide focused training for experienced UNIX administrators on how to install, customize, and administer the AIX operating system in a multiuser POWER (System p) partitioned environment. The course is based on AIX 7.1 running on a Power system managed by Hardware Management Console version 7 and provides practical discussions that are appropriate to earlier AIX releases.

Objectives

  • Install the AIX operating system, filesets, and RedHat Package Manager (RPM) packages
  • Perform system startup and shutdown
  • Discuss and use system management tools such as System Management Interface Tool (SMIT) and IBM Systems Director console for AIX
  • Manage physical and logical devices
  • Discuss the purpose of the logical volume manager
  • Perform logical volume and file system management
  • Perform and restore system backups
  • Use the AIX error log as a tool in problem determination
  • Configure Transmission Control Protocol/Internet Protocol (TCP/IP) networking

Audience

This intermediate course is intended for experienced UNIX system administrators who need training to support their transition to supporting AIX running on POWER processor based systems in a multiuser POWER (System p) partitioned environment.

Prerequisites

You should be able to use basic UNIX commands to:

  • Execute basic AIX commands
  • Manage files and directories
  • Use the vi editor
  • Use redirection, pipes, and tees
  • Use the utilities find and grep
  • Use command and variable substitution
  • Set and change Korn shell variables
  • Write simple shell scripts

The above skills can be acquired by attending AIX Basics (AU130) or (AN100) or through equivalent AIX/UNIX knowledge.

In addition, you are expected to have hands-on experience administering a UNIX operating system (such as Solaris, HP/UX, and others) including:

  • User management and system security
  • Storage
  • Networking
  • System shutdown and restart
  • Backup and recovery
  • System task scheduling

Programme

Day 1

  • Welcome
  • Unit 1: Introduction to AIX and IBM Power systems
  • Exercise 1: Introduction to AIX and IBM Power systems
  • Unit 2: AIX system management tools
  • Exercise 2: Using system management tools in AIX
  • Unit 3: AIX software installation and maintenance
  • Exercise 3: AIX software installation and maintenance
  • Unit 4: System configuration and devices
  • Exercise 4: System configuration and devices

Day 2

  • Unit 5: TCP/IP networking
  • Exercise 5: TCP/IP implementation
  • Unit 6: System startup and shutdown
  • Exercise 6: System startup and shutdown
  • Unit 7: Basics of configuring logical partitions
  • Exercise 7: Configuring logical partitions
  • Unit 8: AIX installation
  • Exercise 8: AIX installation
  • Unit 9: Working with the Logical Volume Manager

Day 3

  • Exercise 9Working with LVM
  • Unit 10: File systems administration
  • Exercise 10: File systems administration
  • Unit 11: The Object Data Manager
  • Exercise 11: The Object Data Manager
  • Unit 12: LVM metadata
  • Exercise 12: LVM metadata issues
  • Unit 13: Disk management procedures
  • Exercise 13: Disk management procedures

Day 4

  • Unit 14: Backup and restore
  • Exercise 14: Backup and restore
  • Unit 15: Error monitoring
  • Exercise 15: Error monitoring
  • Unit 16: System initialization - I
  • Exercise 16: System initialization - I (Parts 1-3)

Day 5

  • Exercise 16: System initialization - I (Part 4)
  • Unit 17: System initialization - II
  • Exercise 17: System initialization - II
  • Unit 18: The AIX system dump facility
  • Exercise 18: System dump
  • Unit 19, Topic 1: Alternate disk installation
  • Exercise 19,Topic 1: Alternate Disk
  • Unit 19, Topic 2: Using multibos
  • Exercise 19: Topic 2: multibos
  • Optional Appendix A: Survey of additional AIX facilities
  • Optional Appendix B: Printers and queues

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

15 mai 2023

Virtual Classroom (GMT / UTC)

BST

English

Instructor Led Online

kr 39 425,00

We also offer sessions in other countries