CODE: ZL1_ES82
LENGTH: 2 day(s)
PRICE: kr15 770,00
This course is designed to provide an understanding of today's complex system mainframe environment on the zEnterprise System and System z servers. It is mainly targeted for operators technical support, system programmers, and any others who need to keep current in this mainframe environment. Through lecture and hands-on exercises, you learn how the hardware and operating systems interact.
This course addresses the following topics:
Describe and categorize the various servers that are commonly found in data centers
Identify and describe workloads that are commonly used on mainframes and distributed servers
Describe a typical data center with multiple server platforms:
Identify when the first IBM general purpose mainframe was introduced
Describe several key IT and mainframe strategies introduced in the 2000s
Identify current and future data center trends
Describe why smarter systems are required to meet future requirements
Introduce the zEnterprise System and describe how it can apply to current and future business requirements
Describe the basic functions, characteristics, and terminology of System z servers
Identify the number of CPs and specialty processors available to various System z servers
List relative performance of recent System z servers as compared to previous servers
Identify and list IBM mainframe servers supporting multiple channel subsystems and z/Architecture
Identify key components of the zEnterprise System and their purpose
Describe and compare various System z components:
Describe and compare I/O infrastructure and processor usage across zEC12 to z10 mainframes
Describe how and what System z physical components are used when processing instructions and performing an I/O operation
Identify System z Capacity on Demand (CoD) options available for planned and unplanned outages
Describe the CoD provisioning architecture and which servers can use it
Describe how logical partitioning is used, resource assignments and initialization activities
Describe mainframe channels, usage, and CHPID assignments
Describe the purpose and use of HCD
Identify mainframe operating systems and their supported mainframe servers:
Describe the difference between a base and Parallel Sysplex
Identify and describe the major enhancements provided by the System z software and hardware platform:
Identify processor architectural modes and their supported addressing implementations:
Describe the various queues that are used to dispatch work
Use system commands to display active address spaces and identify their current status
Describe the high level interaction between z/OS, CSS and I/O devices during I/O processing
Describe the role of the HMC and SE for System z servers
Identify and change the HMC user interface style
Identify CPC and image objects usage on the HMC
Build and customize user-defined groups
Identify profile types, usage and assign profiles to objects
Use the Details window to determine object status and assignments
Describe how and why unacceptable status conditions and hardware messages are presented to the HMC
Identify the HMC activation process for CPCs and images
Send messages to the operating system
The basic class should consist of lead operators, technical support personnel, system programmers, or anyone in the technical field who requires an understanding of how the current hardware and software interact in the large mainframe environment.
You should have an understanding of:
Day 1
Day 2
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show: