CODE: ZL1_AS06
LENGTH: 4 day(s)
PRICE: £2,600.00
Course RPG IV Programming Fundamentals Workshop for IBM i (AS06G) teaches the basics of the IBM i RPG IV programming language. It is the first of two courses that should be attended in sequence.
This course is a comprehensive exposure to the basic features and functions of RPG IV for Version 7. It does not introduce either information processing or programming in general. Students who are new to programming should attend other courses that are offered by local technical colleges or self-study methods.
This course is designed to enable a trained programmer to develop and maintain simple RPG IV programs written using the latest features and techniques available in the Version 7 compiler.
This course is the first in a series of two courses designed for programmers who are new to RPG IV. Basic programming experience is required. The student should have attended at least an introductory course to programming such as one of those available at technical colleges. The student is not taught the concepts of programming.
Experienced programmers who are new to the Power System with IBM i should also attend this course. Examples of other programming languages are BASIC, COBOL, or RPG II.
This course focuses entirely on the features of the RPG IV Version 7 compiler and the techniques that this compiler provides. Features of V7 are discussed.
Previous techniques and the maintenance of programs that are written using legacy techniques, such as fixed format calculations, are not covered in the classroom. Some additional material and the bibliography will assist the new RPG IV programmer in the maintenance of legacy applications.
Roadmaps that reference this course are:
• Application Developer (DB2, WDSc, RPG, CL, SQL) RPG Path
You should be able to:
You must have attended these courses:
Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.
GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf
Once you enroll in a GTP class, you will receive a confirmation letter that should show: