Arrow Electronics, Inc.

IBM MQ V9 System Administration (using Windows for labs)

CODE: ZM153G

LENGTH: 32 Hours

PRICE: £1,140.00

Description

This self-paced course with hands-on exercises provides technical professionals with the skills that are needed to administer IBM MQ queue managers on distributed operating systems and in the Cloud. In addition to the instructor-led lectures, you participate in hands-on lab exercises that are designed to reinforce lecture content. The lab exercises use IBM MQ V9.0, giving you practical experience with tasks such as handling queue recovery, implementing security, and problem determination.

Note: This course does not cover any of the features of MQ for z/OS or MQ for IBM i.

Objectives

After completing this course, you should be able to:

  • Describe the IBM MQ deployment options
  • Plan for the implementation of IBM MQ on-premises or in the Cloud
  • Use IBM MQ commands and the IBM MQ Explorer to create and manage queue managers, queues, and channels
  • Use the IBM MQ sample programs and utilities to test the IBM MQ network
  • Enable a queue manager to exchange messages with another queue manager
  • Configure client connections to a queue manager
  • Use a trigger message and a trigger monitor to start an application to process messages
  • Implement basic queue manager restart and recovery procedures
  • Use IBM MQ troubleshooting tools to identify the cause of a problem in the IBM MQ network
  • Plan for and implement basic IBM MQ security features
  • Use accounting and statistics messages to monitor the activities of an IBM MQ system
  • Define and administer a simple queue manager cluster

Exercises

  • Exercise 1: Using commands to create a queue manager and queues 
  • Exercise 2: Using IBM MQ Explorer to create queue managers and queues 
  • Exercise 3: Using IBM MQ sample programs to test the configuration 
  • Exercise 4: Connecting queue managers 
  • Exercise 5: Connecting an IBM MQ client
  • Exercise 6: Implementing a trigger monitor 
  • Exercise 7: Running an IBM MQ trace 
  • Exercise 8: Controlling access to IBM MQ 
  • Exercise 9: Using a media image to restore a queue 
  • Exercise 10: Backing up and restoring IBM MQ object definitions 
  • Exercise 11: Implementing a basic cluster 
  • Exercise 12: Monitoring IBM MQ for performance 

Audience

This course is designed for technical professionals who require the skills to administer IBM MQ queue managers on distributed operating systems, in the Cloud, or on the IBM MQ Appliance.

Prerequisites

  • Basic knowledge of IBM MQ V9 concepts and features, obtained either through experience or by successfully completing Technical Introduction to IBM MQ (WM103G) or Technical Introduction to IBM MQ (ZM103G)
  • Ability to invoke standard functions within the operating system that is used in the lab exercises
  • Some knowledge of TCP/IP configuration

Programme

  • Course introduction
  • IBM MQ review
  • IBM MQ installation and deployment options
  • Creating a queue manager and queues
  • Exercise: Using commands to create a queue manager and queues
  • Introduction to IBM MQ Explorer
  • Exercise: Using IBM MQ Explorer to create queue managers and queues
  • Testing the IBM MQ implementation
  • Exercise: Using IBM MQ sample programs to test the configuration
  • Implementing distributed queuing
  • Exercise: Connecting queue managers
  • IBM MQ clients
  • Exercise: Connecting an IBM MQ client
  • Implementing trigger messages and monitors
  • Exercise: Implementing a trigger monitor
  • Diagnosing problems
  • Exercise: Running an IBM MQ trace
  • Implementing basic security in IBM MQ
  • Exercise: Controlling access to IBM MQ
  • Backing up and restoring IBM MQ messages and object definitions
  • Exercise: Using a media image to restore a queue
  • Exercise: Backing up and restoring IBM MQ object definitions
  • Introduction to queue manager clusters
  • Exercise: Implementing a basic cluster
  • Monitoring and configuring IBM MQ for performance
  • Exercise: Monitoring IBM MQ for performance
  • Course summary

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:

http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

04 Jun 2023

English

Self Paced Training

£ 1,140.00

We also offer sessions in other countries