Arrow Electronics, Inc.

Db2 11.1 Administration Workshop for Linux - SPVC

Kod: ZL1_2L207

Czas trwania: 4 days

Cena netto: zł3 300,00

Opis szkolenia

Contains PDF course guide, as well as a lab environment where students can work through demonstrations and exercises at their own pace.

This course teaches database administrators to perform basic database administrative tasks using Db2 11.1. These tasks include creating database objects like tables, indexes and views, and loading data into the database with Db2 utilities like LOAD and INGEST. Various diagnostic methods will be presented, including using db2pd command options, and monitoring with SQL statements that reference Db2 monitor functions. Students will learn how to implement automatic archival for database logs and how to recover a database to a specific point in time using the archived logs. The course covers using EXPLAIN tools to review the access plans for SQL statements and adding indexes to improve SQL performance. We will cover the locking performed by Db2 and the effect the application isolation level has on locking and lock wait conditions. Students will learn how to implement database security, including adding a security administrator, SECADM user, and implement database roles to simplify security management. We will also describe implementing Db2 native encryption for a database.

Cel szkolenia

Please refer to course overview

Uczestnicy

This is an intermediate level course for students that will perform Database Administration tasks, who plan, implement, and maintain D22 11.1  databases.

Wymagania wstępne

  • Perform basic database administration tasks on a relational database system
  • Use basic OS functions such as utilities, file permissions, hierarchical file system, commands, and editor
  • State the functions of the Structured Query Language (SQL) and be able to construct DDL, DML, and authorization statements
  • Discuss basic relational database concepts and objects such as tables, indexes, views, and joins

These skills can be developed by taking:

  • DB2 SQL Workshop
  • DB2 Fundamentals

Program szkolenia

• Overview of Db2 11.1
• Db2 Command Line Processor (CLP) and GUI tools
• The Db2 database manager instance
• Creating Databases and Data Placement
• Creating Database Objects
• Moving Data
• Backup and Recovery
• Database Maintenance, Monitoring and Problem Determination
• Locking and concurrency
• Security

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process:

http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Terminy
Date
Location
Time Zone
Language
Type
Guaranteed
Cena netto

04 gru 2021

English

Self Paced Training

zł3 300,00