Arrow Electronics, Inc.

PowerHA SystemMirror 7 Advanced Configurations

Kod: AN62G

Czas trwania: 40 Hours (5 days)

Cena netto: zł9 950,00

Opis szkolenia

This course is designed to teach experienced PowerHA SystemMirror for AIX professionals the latest features in PowerHA SystemMirror. It covers how to:

  • Effectively administer and monitor an IBM PowerHA SystemMirror for AIX cluster
  • Implement PowerHA SystemMirror for AIX's more complex options

Cel szkolenia

  • Review fundamental PowerHA SystemMirror for AIX concepts and components
  • Create four node clusters with two independent resource groups
  • Create and test robust application start and stop scripts
  • Create and test custom application monitors
  • Create resource group dependencies
  • Customize event notifications
  • Integrate WPAR and DLPAR with applications under PowerHA control
  • Integrate applications into PowerHA using Smart Assists
  • Determine the status of the cluster and cluster components using PowerHA/SNMP commands
  • Manage the cluster using the IBM Systems Director plug-in

Uczestnicy

This course is designed for experienced AIX system administrators and support personnel who are responsible for the administration, maintenance, and implementation of PowerHA SystemMirror clusters on IBM Power Systems running AIX. This audience includes:

  • Students who want to learn to work with the PowerHA SystemMirror 7.1 for AIX
  • Students who want to learn about how to implement PowerHA SystemMirror for AIX in complex configurations
  • Technical leaders responsible for designing PowerHA SystemMirror for AIX clustering solutions

Wymagania wstępne

You should have experience with installing and performing standard PowerHA SystemMirror for AIX configuration functions, which can be obtained through the following course (or equivalent experience):

  • PowerHA SystemMirror for AIX System Administration I: Planning and Implementation (AN61G)

You should also be familiar with:

  • The AIX operating system
  • The IBM server hardware that they are using
  • The principles of good system management
  • TCP/IP communications concepts and tools, as covered in (AN12G) or (AN14G) briefly 
  • Logical Volume Manager (LVM) concepts and configuration, as covered in (AN12G) or (AN14G)
  • Good Korn Shell script programming

Program szkolenia

Day 1

  • Welcome
  • Unit 1: PowerHA review with the advanced topology and CSPOC
  • Exercise 1: Lab setup, cluster review, topology, and CSPOC administration

Day 2

  • Unit 2: Adding applications
  • Exercise 2: Adding additional applications

Day 3

  • Unit 3: Advanced administration: Resources and resource groups
  • Exercise 3: Application monitors and resource group dependencies

Day 4

  • Unit 4: Determining cluster status using the command line interface
  • Exercise 4: Determining cluster status using command line Unit 5: Advanced administration: Event configuration Exercise 5: PowerHA for AIX event configuration

Day 5

  • Unit 6: Advanced administration: DLPAR and WPAR implementation
  • Exercise 6: Implementing DLPAR and WPAR
  • Unit 7: Using the PowerHA SystemMirror plug-in for IBM Systems Director (optional)
  • Open lab time

Więcej informacji

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Terminy

We also offer sessions in other countries