Arrow Electronics, Inc.

Advanced Tools for AIX Performance Analysis

CODE: AN52G

LENGTH: 32 Hours (4 days)

PRICE: kr32 380,00

Description

Develop the skills to use kernel traces, trace based utilities, and svmon to measure and analyze CPU, memory, and I/O performance issues on IBM systems running AIX. Reinforce each lecture during extensive hands-on lab exercises and get practical experience applicable to their performance management requirements.

Objectives

  • Use the trace facility to collect data and create a trace report
  • Use the kernel trace facilities to analyze CPU performance issues
  • Describe causes and impacts of high context switching rates
  • Identify what causes a thread to be blocked and later woken up
  • Explain the relationship between the output of svmon -G, svmon -P, and svmon -S
  • Calculate the amount of memory in use on the system
  • Explain the relationship between svmon, vmstat, and ipcs output
  • Categorize the memory in use on the system by segment type
  • Identify which processes are using the most memory or paging space
  • Describe the characteristics of asynchronous I/O, synchronous I/O, direct I/O, and concurrent I/O
  • Identify if the expected type of I/O is being executed
  • Tune asynchronous I/O

Audience

The audience for this training includes AIX technical support personnel, performance benchmark personnel, and AIX system administrators.

Prerequisites

You are expected to have extensive AIX skills. These skills can be obtained by attending the following courses:

  • AIX Power Systems for AIX IV: Performance Management (AN510) or have the equivalent extensive AIX skills

Programme

Day 1

  • Welcome
  • Unit 1: AIX trace facilities
  • Exercise 1: AIX trace facilities
  • Unit 2: Advanced memory topics - I
  • Exercise 1: AIX trace facilities (Part 3)
  • Exercise 2: Advanced memory topics - I

Day 2

  • Unit 3: Advanced memory topics - II
  • Exercise 3: Advanced memory tropics - II
  • Unit 4: Advanced CPU topics - I
  • Exercise 4: Advanced CPU topics - I
  • (Optional) Exercise 4: Advanced CPU topics - I (Part 2)

Day 3

  • Unit 5: Advanced CPU topics - II
  • Exercise 5: Advanced CPU topics - II
  • Unit 6: Advanced I/O topics - I
  • Exercise 6: Advanced I/O topics - I (Part 1)
  • (Optional) Exercise 5: Advanced CPU topics - II
  • (Parts 2 and 3)

Day 4

  • Exercise 6: Advanced I/O topics - I (Part 2)
  • Unit 7: Advanced I/O topics - II
  • Exercise 7: Advanced I/O topics - II
  • (Optional) Exercise 7: Advanced I/O topics - II (Part 3)

Further Information

Prior to enrolling, IBM Employees must follow their Division/Department processes to obtain approval to attend this public training class. Failure to follow Division/Department approval processes may result in the IBM Employee being personally responsible for the class charges.

GBS practitioners that use the EViTA system for requesting external training should use that same process for this course. Go to the EViTA site to start this process: http://w3.ibm.com/services/gbs/evita/BCSVTEnrl.nsf

Once you enroll in a GTP class, you will receive a confirmation letter that should show:

  • The current GTP list price
  • The 20% discounted price available to IBMers. This is the price you will be invoiced for the class.

Session Dates
Date
Location
Time Zone
Language
Type
Guaranteed
PRICE

10 jul 2023

Virtual Classroom (GMT+1)

CEDT

English

Instructor Led Online

kr 32 380,00

We also offer sessions in other countries