Kód: SOP_FCEACH
DÉLKA: 3 (den)
CENA: Kč 45 300,00
Školení je vedeno virtuálně v anglickém jazyce.
Cena školení je 1 500 GBP bez DPH - tato cena bude při fakturaci přepočtena aktuálním kurzem.
The course is intended to be delivered in a classroom setting and consists of presentations and practical lab exercises to reinforce the taught content. Copies of the supporting documents for the course will be provided to each trainee.
Due to the nature of delivery, and the varying experiences of the trainees, open discussion is encouraged during the training.
The course is expected to take 3 days (24 hours) to complete, of which approximately 8 hours will be spent on the practical exercises.
On completion of this course, trainees will be able to:
Deploy Sophos Firewall in complex network environments
Explain how Sophos Firewall processes traffic and use this information to inform the configuration
Configure advanced networking and protection features
Protect web applications using the web server protection
Size hardware, virtual and software Sophos Firewalls for a given set of requirements
This course provides an in-depth study of Sophos Firewall, designed for experienced technical professionals who will be planning, installing, configuring and supporting deployments in production environments.
Prior to taking this training, you should:
Have completed and passed the Sophos Firewall Certified Engineer course and any subsequent delta modules up to version 18.5
We recommend students have the following knowledge and experience:
Experience with Windows networking and the ability to troubleshoot issues
A good understanding of IT security
Experience configuring network security devices
Experience configuring and administering Linux/UNIX systems
If you are uncertain whether you meet the necessary prerequisites to take this course, please email us at globaltraining@sophos.com and we will be happy to help.
Module 1: Deployment (70 mins)
Recall important information from the Engineer course
Describe the deployment modes supported by the Sophos Firewall
Understand a range of scenarios where each deployment mode would commonly be used
Use built-in tools to troubleshoot issues
Labs (5 mins)
Register for a Sophos Central evaluation
Module 2: Base Firewall (120 mins)
Explain how the Sophos firewall can be accessed
Understand the types of interfaces that can be created
Understand the benefits of Fast Path technology
Configure routing per firewall rule
Understand best practice for ordering firewall rules
Explain what Local NAT policy is and known how to configure it
Labs (120 mins)
Activate the Sophos Firewalls
Post-installation configuration
Bridge interfaces
Create a NAT rule to load-balance access to servers
Create a local NAT policy
Configure routing using multiple WAN links
Configure policy-based routing for an MPLS Scenario
Install Sophos Central
Module 3: Network Protection (45 mins)
Explain what IPS is and how traffic can be offloaded to FastPath
Demonstrate how to optimize workload by configuring IPS policies
Examine advanced Intrusion Prevention and optimize policies
Configure advanced DoS Protection rules
Demonstrate how the strict policy can be used to protect networks
Labs (15 mins)
Create advanced DoS Rules
Module 4: Synchronized Security (45 mins)
Explain how Security Heartbeat works
Configure Synchronized Security
Deploy Synchronized Security in discover and inline modes
Understand the advantages and disadvantages of deploying Synchronized Security in different scenarios
Labs (40 mins)
Configure source-based Security Heartbeat firewall rules
Destination-based Security Heartbeat
Missing Security Heartbeat
Lateral Movement Protection
Module 5: Web Server Protection (60 mins)
Explain how Web Server Protection works
Describe the protection features
Configure protection policies for a web application
Configure web server authentication
Publish a web service using the Web Application Firewall
Use the preconfigured templates to configure Web Server Protection for common purposes
Configure SlowHTTP protection
Labs (90 mins)
Web Application Firewall
Load balancing with Web Server Protection
Web Server Authentication and path-specific routing
Module 6: Site-to-Site Connections (90 mins)
Configure and deploy site-to-site VPNs in a wide range of environments
Implement IPsec NATing and failover
Check and modify route precedence
Create RED tunnels between Sophos Firewalls
Understand when to use RED
Labs (90 mins)
Create an IPsec site-to-site VPN
Configure VPN network NATing
Configure VPN failover
Enable RED on the Sophos Firewall
Create a RED tunnel between two Sophos Firewalls
Configure routing for the RED tunnel
Configure route-based VPN
Module 7: Authentication (40 mins)
Demonstrate how to configure and use RADIUS accounting
Deploy STAS in large and complex environments
Configure SATC and STAS together
Configure Secure LDAP and identify the different secure connections available
Labs (30 mins)
Configure an Active Directory authentication server
Configure single sign-on using STAS
Authenticate users over a Site-to-Site VPN
Module 8: Web Protection (50 mins)
Choose the most appropriate type for web protection in different deployment scenarios
Enable web filtering using the DPI engine or legacy web proxy
Configure TLS inspection using the DPI engine or legacy web proxy
Labs (25 mins)
Install the SSL CA certificate
Configure TLS inspection rules
Create a custom web policy for users
Module 9: Wireless (45 mins)
Explain how Sophos Access Points are deployed and identify some common issues that may be encountered
Configure RADIUS authentication
Configure a mesh network
Module 10: Remote Access (20 mins)
Configure Sophos Connect and manage the configuration using Sophos Connect Admin
Configure an IPsec remote access VPN
Configure an L2TP remote access VPN for mobile devices
Labs (30 mins)
Sophos Connect
Module 11: High Availability (60 mins)
Explain what HA is and how it operates
Demonstrate how to configure HA and explain the difference between quick and manual configuration
List the prerequisites for high availability
Perform troubleshooting steps and check the logs to ensure that HA is set up correctly
Explain the packet flow in high availability
Demonstrate how to disable HA
Labs (20 mins)
Create an Active-Passive cluster
Disable High Availability
Module 12: Public Cloud (45 mins)
Explain how Sophos Firewall fits into public cloud security architect
Deploy a Sophos Firewall on Azure and AWS
Configure Sophos Firewall for hybrid deployments
Deploy a high availability pair of Sophos Firewalls on Azure and AWS
Labs (45 mins)
Put a service in debug mode to gather logs
Retrieving log files
Troubleshoot an issue from an imported configuration file
Deploy a Sophos Firewall on Azure (Simulation)
Deploy a Sophos Firewall on AWS (Simulation)
To become a Sophos Certified Architect, trainees must take and pass an online assessment. The assessment tests their knowledge of both the presented and practical content. The pass mark for the assessment is 80% and is limited to 3 attempts.